Hi Jianxiong,
Hua Jianxiong said: I'm working on TDA4APE with sdk11.0 to do ISP tunning for a raw12 traffic sensor (OV OG12A sensor). The images of this sensor are combined of HCG and LCG frames, and the PWL in sensor is 16 bit to 12 bit.
Do you mean…
Part Number: TDA4APE-Q1 Hi experts,
We are developing a board based on the TDA4APE and we use the DRV8889 Stepper Driver chip to achieve focus adjustment of the camera. Communication and control between the TDA4APE and the DRV8889 are done via SPI.…
Part Number: TDA4AP-Q1 Other Parts Discussed in Thread: AM5728 Tool/software: Hi,
In the below thread, I have selected a part number, do i have to purchase a seperate OS for DO178B if so then the same can be done with AM5728
e2e.ti.com/.../589815…
Part Number: TDA4APE-Q1 Tool/software: Hi TI experts,
We plan to use CCS to debug APE, but the 12.7.0 version does not have the necessary device support. We would like to inquire whether CCS supports APE and, if so, in which version?
Thanks in advance…
Part Number: TDA4APE-Q1 Tool/software: Hey
I have a question about the RMII clock configuration on P379 of the TRM.
The RMII clock configuration consists of Figure 5-23(a) and (b), but the document states that (a) configuration is not supported. …
Part Number: TDA4APE-Q1 Tool/software: Hello Experts,
My understanding is that DMA transfer is possible with OSPI and LPDDR4, but looking at TRM, it seems impossible. Please confirm if it is possible?
If not possible, do we need to connect to…
Part Number: TDA4AP-Q1 Tool/software: Hi,
I am working on a custom board based on the TDA4 chip, aiming to enable the McASP interface in I2S mode. The TDA4 should generate both clocks on the MCASP0_ACLKR and MCASP0_AFSR pins. The TDA4 only receives…
Part Number: TDA4AP-Q1
Tool/software:
Hi, how can you trap floating point exceptions on linux? We tried to use feenableexcept() but it failed for every exception bit. We looked into the ARM A72 doc, but it says, it is not supported. Is there any way…
Part Number: TDA4APE-Q1 Tool/software: Hardware: TDA4APE SDK: 1001 linux + RTOS
We want to know whether uboot supports the ums command on the TDA4APE platform? we found that the ums command is not supported under the precompiled U-boot.
Part Number: TDA4APE-Q1 Tool/software: TDA4APE custom board
SDK 11.0
freertos+linux
The theoretical DDR bandwidth of our board is 4266M * 32 * 2 / 8 = 34GB/s.
We found that when all the cameras were functioning properly, the average bandwidth…