Part Number: TDA4VE-Q1 Dear TI Engineer,
I have few questions related with the TDMA4VE SoC
In the E2E, you've mentioned to place CPSW2G under A72 Linux and change the networking rule to forward packet.
Does this mean to just packet forwarding form…
Part Number: TDA4VE-Q1 Other Parts Discussed in Thread: TPS65223 , TPS62873-Q1
Hi sir,
Here is a question, in PDN-7G v0.22 BUCK4 power rail net name is 0.75V, but in Jacinto7 J722S Pwr Sols v1.0 in page 13, there write BUCK4 is 0.85V and current is 3mA…
Part Number: TDA4VE-Q1 Other Parts Discussed in Thread: TDA4VM Hello Experts,
Since there is only C7x type DSP in TDA4VE, but in SDK 0806 there are some c66 typed kernels and targes.
According to the datasheet that C7x in TDA4VE should be 5 times faster…
Part Number: TDA4VE-Q1 Hello, TI experts.
We are currently designing a system using the TDA4V mid eco, planning to run Autosar on the MCU domain and QNX on the main domain.
We intend to develop using SDK version 9.X. Our system configuration will connect…
Part Number: TDA4VE-Q1 Hi TI Experts,
In our production, we plan to use different sensor of camera for 9 cameras input on TDA4VE and TDA4VEN.
We'd like to know if there is any limitation of that? Can we support it simultaneously.
For example,
4*…
Part Number: TDA4VE-Q1
Hi, Im developing ADAS PRK1.5A ECU using TDA4VE.
Because of board size, eMMC has to be far from the AP.
Do you have any restriction of eMMC Signal legnth?
Part Number: TDA4VE-Q1 Hi TI experts:
I recompiled the kernel Image as following steps:
1. cd [path-to-linux-SDK-root-path]
2. run "make linux "
And I got the "Image" file under board_support/ti-processor-sdk-linux-adas-j721s2…
Part Number: TDA4VE-Q1 Hi, TI
Does TDA4VMEco supports SGMII interface?
on datasheet and TRM, There was no metion whether AP support sgmii interface or not.
But on schematic checklist, It saids AP can support SGMII.
Best regards,
Part Number: TDA4VE-Q1 Hi Expert,
We use J721S2 and PSDK8.4,
Currently our target board can display via DSI, And originally the AB26 & AD28 pin are configured to I2C.
After configuring AB26 & AD28 to the UART of A72 Linux, the user application access…
Part Number: TDA4VE-Q1 Hello Ti support:
I am going to find some TDA4V Entry (PN: TDA4VEN) documents and relation SDK, but I cannot find any data in TI website.
could you give me some information?
Thinks