Part Number: TDA4VE-Q1 Hi expert,
Due to some structure limitation, our customer cannot follow the DDR placement of EVM and have to move one DDR from left side to the bottom side as shown below. Our customer would like to know:
1. they can ensure each…
Part Number: TDA4VE-Q1 Hi TI,
on PDN-3F,
what is FFI means?
Should we do something setting, when we want to use MCU booting?
if we use PDN-3F,
when AP Core supply downs but MCU Supply still alives,
Can AP's MCU alive?
Best regards,
Part Number: TDA4VE-Q1 Hi TI,
On datasheet 500Ohm +-1% resistor was recommended for CSI on-chip calibration resistor (CSI0_RXRCALIB)
However, on EVM sch. I think TI used 499ohm resistor.
if 500ohm +-1%, it's tolerance values is 495 ~ 505ohm…
Part Number: TDA4VE-Q1 I couldn't find the root code of "UART_printf" at the "ipc_trace.c" in PDK of "ti-processor-sdk-rtos-j721s2-evm-09_01_00_06":
So where is it so that I could figure out the details of uart pins…
Part Number: TDA4VE-Q1 Other Parts Discussed in Thread: TDA4VM Hi, TI team.
WKUP_GPIO0_6 is connected to TP45 (Test point) in TDA4VM(J721E) EVM.
My colleague used WKUP_GPIO0_6 to control Pin by setting the register like below:
Configure WKUP_GPIO0_6…
Part Number: TDA4VE-Q1 Hello experts,
I have questions about TDA4VE-Q1 Boot mode [15:14] and would like your help.
According to TRM, Boot mode [15:14] is reserved. Is the setting of Boot mode [15:14] the same for G version and 0 version?
Can we set…
Part Number: TDA4VE-Q1 Hello TI Team,
I want to generate the LDC LUT file for the DCC-Tool with the camera Matrix and the Coefficients which I calculated using openCV.
The DeWarping with openCV looks good but if I use the correction values from "mapx…
Part Number: TDA4VE-Q1
Hi,
We are currently using the TDA4VE Linux SDK 9.1, and GStreamer to encode a few video streams, as an evaluation of the mentioned chip.
We are very interested into advanced encoder features that are provided by the SoC hardware…
Part Number: TDA4VE-Q1 ti-processor-sdk-rtos-j721s2-evm-08_06_01_03 and ti-processor-sdk-rtos-j721e-evm-07_03_00_07
img_proc_pipeline_blocks_nv12ToRgbp in ti-processor-sdk-rtos- j721s2-evm-08_06_01_03 /vision_apps/kernels/img_proc/c66/vx_image_preprocessing_target…