Part Number: TDA4VM Hello, experts:
Our problem: After we call the post-board end reasoning results and save them to a file, the PC parsing and visualization do not match the expected results. Our expectation: We hope to find the reason for the incorrect…
Part Number: TDA4VM Hi TI Expert,
Can the following operations be implemented under HSM/TEE? If so, are these operations performed by the MCU domain or the MAIN domain?
1. Verify storage by sending FoD Cert with correct signature to the HSM 2. Check…
Part Number: TDA4VM Tool/software: Hi,
I am using TDA4VM for object detection and tracking, from the model zoo i can figure out that tda4vm support object detection model, dose is support track model?Such
as ByteTrack model? if it does not support…
Part Number: TDA4VM kernel: Linux version 6.12.17-ti-00781-g95010a7c186b (oe-user@oe-host) (aarch64-poky-linux-gcc (GCC) 13.3.0, GNU
After loading freertos_test_task_switch_c66xdsp_1_release.xe66 and linking to it from /lib/firmware
The firmware was…
Part Number: TDA4VM Hi, I was wondering if there was any method to run transformer based models on the TDA4VM platform. I want to be able to run flash attention for my problem statement. I have noticed that the model compiler says that transformer model…
Part Number: TDA4VM All,
This thread has taken place on internal e2e, moving to external e2e to continue the discussion between TI and the customer.
TI Internal thread is here:
1578643/tda4vm-fails-to-allow-the-a72-cores-to-finish-loading-tispl…
Part Number: TDA4VM Tool/software: Hello Team,
I have a video pipeline application which makes use of tensorflow model and the algorithm has dependencies on OpenCV. Can you please guide in porting this application into TDA4VM?
Best Regards
Ch…
Part Number: TDA4VM-Q1 hello there,
in ourADAS L2+ domian application, SOC MPN is TDA4VM88T5CALFRQ1 , a return part from OEM with Zero-kilometer indicates that the SOC failed to startup. And we can reoccur this fault in our labaritory with 8/10 probability…
Part Number: TDA4VM Other Parts Discussed in Thread: CCSTUDIO
I spent a while trying to connect to a core in the TDA4VM SoC using TDA4VM-SK starter kit and the xds110 debug probe I recently purchased.
I have already checked : https://e2e.ti.com/support…
Part Number: TDA4VM Dear experts,
I installed Debian 13 onto SK-TDA4VM. But I've found that the display cannot be hardware accelerated because the OpenGL in Debian 13 cannot use the GPU within SK-TDA4VM.
The renderer used by the system is "llvmpipe…