Part Number: TDA4VM-Q1 Dears,
we have several temperature sensor in TDA4x
How to check which temperature sensor on which area of Soc? Thanks
Regards,
Fredy Zhang
Hi Xie,
xie jc said: I can really run kyewriter on HS-SE dvice, although i will see errors, i can at least see print from the serial output. (As you said, the key must be matched)
KeyWriter is intended to be run _only_ on a HS-FS device to convert it to…
Part Number: TDA4VM-Q1 We use 2 TDA4s for Ethernet communication, SDK version 8.6. Two TDA4 eth0 nics on Linux based on undivided VLAN, Run the ‘ip link add link eth0 name eth0.3 type vlan id 3’ command to create network adapter eth0.3 on VLAN3.…
Hi Tahm,
xie jc said: Do you mean that after the modification, every frame encoded as h.264 is an IDR frame? Or are you saying that each frame contains one IDR frame?
Enabling this will encode every frame as an IDR frame. This will ensure header information…
Part Number: TDA4VM-Q1 Other Parts Discussed in Thread: TDA4VM Hi Expert,
1.It is necessary to configure the corresponding interruption number for the route, but I am a little confused about filling in the interruption number. In the J721E technical reference…
Part Number: TDA4VM-Q1 Other Parts Discussed in Thread: TDA4VH Hello,
Our app has been running on TDA4VH with rtos sdk 0703 for a long time, recently, we found someie error in capture node statistics, shown as below:
2024-04-09 16:33:29 [MCU2_0] 44524…
Part Number: TDA4VM-Q1
Hi TI expert,
As title description.
TDA4VM-Q1 USB1 to be a slave role connected with Hub's downstream port. Hub chip is using Genesys GL852.
When Hub power source selection VS USB idle state:
Bus power- Because USB idle state…
Part Number: TDA4VM-Q1
Hi, Ti engineers,
I try to test display node on EVM board. the chain links: read_picture -> display->node, but get an error, can you git me some guides to solve this problem.
SDK version: 8.4
Regards
Tahm