Part Number: TDA4VM-Q1 Hi, expert
Do GPU have any restrictions of input size of texture, like length or bandh must be multiple of 64 pixel?
Regards
Zekun
Part Number: TDA4VM-Q1 HI, expert
I use python to parse uart log from HS board but failed. I want to know the keywriter status. Please share some ideas.
parse_uart_boot_socid_update(1).py
#!/usr/bin/env python3
import binascii
import struct…
Part Number: TDA4VM-Q1
Hello Team,
We understard there is internal monitoring of temperatures in TDA4 and gives warning when reached threshold and it can reset if temperature reached cutoff.
once the cutoff temperature is reached, reset reason we do…
Part Number: TDA4VM-Q1 Hello TI engineers,
Due to project requirements, we are planning to use hwa encode. We want to understand how to use hardware encoding by running the demo app_multi_cam_codec. However, we only have the EVM board without a camera…
Part Number: TDA4VM-Q1 Other Parts Discussed in Thread: TDA4VM Dear,
I am building the "Processor SDK Linux for J721e 09_01_00" in your site. ( https://software-dl.ti.com/jacinto7/esd/processor-sdk-linux-jacinto7/latest/exports/docs/linux/Overview_Building_the_SDK…
Part Number: TDA4VM-Q1 Other Parts Discussed in Thread: SK-TDA4VM , TDA4VM Hi TI expert,
Please help to confirm below question:
1-Warm reset supprt or not in SK-TDA4VM EVM.
2--J7 EVM warm reset was trigged by RESET_REQZ. Is right or wrong...
3-If warm reset…
Part Number: TDA4VM-Q1 Other Parts Discussed in Thread: DS90UB913A-Q1 , DS90UB964-Q1EVM
Dear Sir,
I am working with
PSDK 08_02_00_05
Serializer: DS90UB913A-Q1 (ISX016)
Deserializer: DS90UB964-Q1EVM
Last Friday, we tested the application and it was working…
Part Number: TDA4VM-Q1
Hi TI expert,
Product is default configured in eMMC boot not SD boot.
SDK version: 08.01.00.006.
Issue description:
After cold reset we sometimes met filesystem mounting fail. Because mmcblk1 initialized earlier than mmcblk0 in…
Part Number: TDA4VM-Q1 Other Parts Discussed in Thread: TDA4VM , TDA4VH Hi Expert,
What PCIE_REFCLK level standards can TDA4VH and TDA4VM support, I know we can support HCSL, how about others such as LVCMOS, and LVDS?
BR,
Biao