Part Number: TDC1000-C2000EVM Other Parts Discussed in Thread: TDC1000 , MSP430FR6043 , TDC7200 Hello all, I have a question.
I would like to use a TDC1000-C2000EVM and two 2 MHz transducers to detect the flow rate of tap water flowing through a PVC pipe…
Part Number: TDC1000 Other Parts Discussed in Thread: TUSS4470 , PGA460 , Can this chip be used for level sensing on small fluid bottle 5.5 inch (140 mm) ?
Part Number: TDC1000 Hello,
I was looking at the TIDA00322EVM reference design and in the test results it calls out a guide called "TIDA00322EVM – Quick Start Guide.pdf " on how to load the GUI application onto that board. I have been unable to find the…
Part Number: TDC1000 hi,
In TDC1000 we are planning to use the mode 2 for water flow measuring application,
it is mentioned in the data sheet, "TX1,RX2 is one pair & TX2,RX1 is another pair" so, needs 2 transmitter and 2 Receiver, if the…
Part Number: TDC7200 Other Parts Discussed in Thread: TDC1000 , , MSP430FR6047
Hello,
I'm working on a project to develop an ultrasonic flowmeter using the time of flight (TOF) method. I'm using 2 transducers (2 MHz), TDC1000 (AFE) and TDC7200. I am also…
Part Number: TDC1000 if we directly connect the received signal from transducer(avoiding LNA and PGA) to compin, directly do we have to place any filter inbetween LNAOUT and COMPIN,if yes which kind of filter can be used?
Part Number: TDC1000 Other Parts Discussed in Thread: PGA460 , TDC7200 , DRV8870 Hello,
I am trying to find a good solution to measure the depth of the water using an Airmar P19 depth transducer, which is mounted on a sailing boat, few cm under the floating…
Part Number: TDC1000 Other Parts Discussed in Thread: PGA460 , TUSS4470
Looking for piezo cermaic transducers for liquid level sensing if a few different freqs but having trouble finding them. I'm looking for a few different piezo ceramic disks with a…
Hello Isaac,
Thanks very much. Yes, the RTD interface is on the TDC1000. I wrote the configurations into the registers of TDC1000, and I got the START and STOP signals out from TDC1000 pins. Below listed the scope time of RTD measurement, and I think…