Part Number: TDC1000 Other Parts Discussed in Thread: TDC7200 , EVM430-FR6047 , MSP430FR6047 Hello,
We are a team that has developed a contactless water speed measurement system in a pipe, using Audiowell ultrasonic probes arranged in a V configuration…
Hello Esteban,
Thanks for the background on this. If you are working with water I believe your transducer frequency is rather low from what we typically see on these types of applications. Typically we see 1MHz transducer frequency but the distances are…
Part Number: PGA308 Other Parts Discussed in Thread: TDC1000 Tool/software: dear sir
our customer want PGA308 with TDC1000 due to very pricision output control.
for test, customer 2MHz sensor signal input to TDC1000, unfortunately, PGA308 output can…
Part Number: TDC1000-C2000EVM Other Parts Discussed in Thread: TDC1000 Tool/software: Hello!
I am looking for a method to have more flexibility over the clock speed of the TDC1000 chip. Is there any way that the evaluation board can be manipulated so…
Part Number: TDC1000 Tool/software: hi, our customer want know "Vcom" function..
Ti data sheet describe that "should not be loaded with more than 20 μA.".
If this pin loaded over 20uA, what happen TDC1000.
please help!
Hello Archie,
i want to ask if i can add booster to the development kit which i have (TDC1000-C2000EVM) , to measure the range 2 meters , instead of buying new Kit?
Yes you can add a booster to the current EVM. That would be closer to this EVM that…
Part Number: TDC1000 Other Parts Discussed in Thread: TUSS4470 , PGA460 , Can this chip be used for level sensing on small fluid bottle 5.5 inch (140 mm) ?
Part Number: TDC1000-C2000EVM Other Parts Discussed in Thread: TDC1000 , MSP430FR6043 , TDC7200 Hello all, I have a question.
I would like to use a TDC1000-C2000EVM and two 2 MHz transducers to detect the flow rate of tap water flowing through a PVC pipe…
Part Number: TDC1000-C2000EVM Tool/software:
I have the above configurations and I am trying to find the TOF that I can feed into the formula, D=(TOF X speed of sound)/2 to get the length of the container but even when I change the position of the transducer…