Other Parts Discussed in Thread: TDC7200 , TDC1011 , TDC1000 Dear all,
Currently, I'm using TDC1011, TDC7200 and SMFM21F1000 to detect existence and nonexistence of water in a water tank , the width is 40cm , for a cow. The excitation specification is…
Other Parts Discussed in Thread: CC2640 , TDC1011 Hi,
I'm planning to use CC2640 with TDC1011. In one of the application note, TMS320F28035-Q is suggested to be used with TDC1011 as it has 300ps accuracy. In my application, I need the level sensing accuracy…
Other Parts Discussed in Thread: PGA460 , TUSS4470 , MSP430FR6047 , TUSS4440 , BOOSTXL-PGA460 , BOOSTXL-TUSS4470 , EVM430-FR6047 , BOOSTXL-TUSS4440 , TDC1000 , TDC1011 Ultrasonic sensing uses the propagating sound waves at a frequency above the range of human hearing…
Other Parts Discussed in Thread: TDC1000 , TDC1011 Hello, In introductory videos of TDC1000 and TDC1011, Single transducer is being used for level sensing of water(No separate Rx and Tx). I am having pair of transducers (Tx and Rx), Can I use these transducers…
Other Parts Discussed in Thread: CC2640 Hi,
I'm planning to use CC2640 with TDC1011 . In one of the application note, TMS320F28035-Q is suggested to be used with TDC1011 as it has 300ps accuracy. In my application, I need the level sensing accuracy of up…
Other Parts Discussed in Thread: TDC1000 , TDC1011 , TDC1000-C2000EVM Hello everyone
Can someone help me if I can use TDC1000 or TDC1011 for medical applications? I want to measure the distance of body tissues from the surface( skin) and find the movement…
Other Parts Discussed in Thread: CC2640 , TDC1011 Hi All,
Using CC2640, I need to generate a clock source of 1MHz for a external sensor, can any one help me with that and suggest me a example code for the same ?
Thanks
Brajesh
Part Number: TDC1000 Other Parts Discussed in Thread: TDC7200 , TDC1011 , TDC7201 , MSP430F5528 , , TDC7200EVM , MSP-EXP430F5529LP , TDC7201-ZAX-EVM ,
For liquid-coupled ultrasonic sensing applications including level sensing, fluid contamination and identification…
Dear All,
I'm reading in TIDA-00322 Test Results , Paragraph IV / Point B.2. : Connect the transducer TX/RX wire to J3.P8, and the sensor's ground to J3.P10.
According to Schematic/Block Diagram , connecting the transducer between P8 and P10 leads…
Other Parts Discussed in Thread: PGA450-Q1 , PGA450Q1EVM Dear all,
We are experiencing difficulties in selecting the right IC for our application. Can someone help us in this regard?
We need to measure distances from 50cm to 2m; and up to 15m for an extended…