Part Number: TDC7200 Other Parts Discussed in Thread: TDC7201 Tool/software: Hi,
My customer is considering TDC-GPX2.
I Proposed TDC7200, but they said that the number of channels is small. Could you tell me the product with 4 channels as an alternative…
Part Number: TDC7200 Other Parts Discussed in Thread: TDC1000 , , MSP430FR6047
Hello,
I'm working on a project to develop an ultrasonic flowmeter using the time of flight (TOF) method. I'm using 2 transducers (2 MHz), TDC1000 (AFE) and TDC7200. I am also…
Part Number: TDC7200 I have made a few test and is it normal that the stop pulse is not taking into account if it's inside the start pulse ?
If that's the case, do you have a work around ? or should I adapt my application somehow ?
yellow is…
Part Number: TDC7200
Tool/software:
I have a custom encoder project where I want to measure the time between three gates monitored by IR TX and RX points, Couple of questions around the circuit above
1) My average pulse durations between start signal…
Other Parts Discussed in Thread: TDC7200 I am developing an ultrasonic meter for a company and need a sample of time to digital IC. I was thinking about tdc7200 and would like to test this IC in the design. It is possible?
Part Number: TDC7200 Other Parts Discussed in Thread: TDC7201 , SN74LS31 , OPA3690 I am building a circuit with comparator and TDC7200. I would like to avoid the 12ns deadtime. Can you offer a suggestion for an IC to delay the pulse by 12 to 15ns, that…
Part Number: TDC7200 Hello! I am using TDC7200 TOF sensor witg 32 cycles averaging and measurement mode 2.
Datasheet states that clock counter should be shifted by log2(AVG_CYCLES) in multi cycle averaging.
My understanding is that the original result…
Part Number: TDC7200 Hello,
Would it be possible to unlock this thread?
e2e.ti.com/.../
After a month I come back to this issue but the thread is locked. I'd like to add new findings.
Thanks.
Dan
Hello,
I finally located the underlying issue. There were two flaws in my code handling TDC7200 measurements: A) The code reads all TIME registers in one read command using "auto-increment" to speed up transfer. However, I got the number of bytes to read…
Part Number: TDC7200EVM Other Parts Discussed in Thread: UNIFLASH , TDC7200 I have been trying to use the TDC7200EVM and accompanying GUI to perform TDC-based ToF measurements, and I am running into a major hurdle. I have procured a MSP430F5529LP (the…