Part Number: TDP0604 Tool/software: Hi sir,
My customer use TDP0604 at their video host application. In their test, they modify GPIO setting to fix video flashing question at high resolution (4K 60Hz).
In their experiment, they pull high mode pin…
Part Number: TDP0604 We are operating the TDP0604IRNQT in I2C mode for DisplayPort. Do the TDP0604IRNQT TX transmitters need to be externally AC coupled ? It is not clear from the datasheet. Since we are in I2C mode, configuration is via the registers…
Part Number: TDP0604 Other Parts Discussed in Thread: SN65DP159 Hi
Can this TDP0604 support DVI1.0 output? My application is DVI1.0 output from DP++ input.
Thanks.
Part Number: TDP0604 Other Parts Discussed in Thread: SN65DP159 Hi team,
Please advise me on my question bellow.
Question:
If TDP0604 has a clock recovery circuit, when it is used in limited mode with HDMI2.0 use case?
Mita
Part Number: TDP0604 HI TEAM
I want to ask if there is a problem with my current design?
Please see the attachment
UBIQCONN_HDMI Level Shift Hybrid redrive_ted0604i_20230314_01.pdf
Part Number: TDP0604 Hi,
I am using TDP0604 as an HDMI retimer in a video monitor and have two questions.
Question 1. There may be a case that HDMI signal is applied to the device while the DC power of the device is off. I am concerned that the current…
Part Number: TDP0604 Hi,
I had design TDP0604 for HDMI2.0 output.
I set control method to I2C control mode.
But I did not find these parameter default value. Please help to provide this information, thanks.
1) Lane swap. Normal or reverse
2) Receiver…
Part Number: TDP0604 Hello,
I have a TDP0604 in a DP tp DP linear redriver configuration set over I2C. I am trying to tune the EQ settings for my losses on board via I2C registers. The register sets have explicit 0-15 bit for EQ settings on lanes D0-D2…