Part Number: TDP158 Other Parts Discussed in Thread: HD3SS3412 Hi
Customer is studying TDP158RSB for HDMI 2.0
Coud you help to support the layout inquiries below
1) Max trace length into redriver, out of redriver
2) Recommended trace impedance
3) Recommended…
Part Number: TDP158 Hello Sir:
We want to setup TDP158 for HDMI 2.0 interface.
And we setup address 0Bh to 5B, 0Ch to 60 and 0Dh to 78.
Can you remind us if using on HDMI 2.0 which address value should be modified too?
Please help to provide your recommendations…
Part Number: TDP158 Other Parts Discussed in Thread: TMDS181 , TMDS171 Hi Team,
My customer read the TDP158 datasheet and find, in the DDC snoop section, we only have the recommendation on the DDC snoop on source side, but there is nothing on sink side…
Part Number: TDP158 Hi Team,
I have one customer, it is their first time to use TDP158 , as they had followed the datasheet, but they still want to get the confirmation from TI BU, please help to check.
Part Number: TDP158 Team,
In the datasheet of TDP158, the power down current is 7mA, same with the standby current, it is x100 times higher than the competitors part. Is it true? Or typo?
Best Regards,
Peter Wei
Part Number: TDP158 Hi,
I used DP dual mode as input source, and HDMI connector output,
But system detect it is DVI output, so resolution only FHD. I used NVIDIA GPU , Monitor is DELL P2415Q.
Is possibly TDP158 send wrong EDID to GPU? Is there need any special…
Part Number: TDP158 Hello sir:
We are using TDP158.
And we are testing HDMI 1.4, and we provide our tested report for you reference.
We only change the register 0C to 60 and register 0D to 78, and the other registers are using default value.
And according…
Part Number: TDP158 Other Parts Discussed in Thread: LMH1297 , LMH0324 Hi,
May I know TI have any Long rang image transfer solution? >100m is better.
Thanks!
Jeff