Hi Mark,
Entering test mode after power up (assuming the references are settled) is no problem, and you could certainly use this as a calibration scheme. After exiting test mode, you can write the desired values to the configuration registers and proceed…
Part Number: THS1206M Hi
Our customer is looking for the Maximum Junction Temp (deg C) as well as the Thermal Resistance Junction to Board (deg C/W) of THS1206M (5962-9957701NXD).
I am hoping you could help us to provide the information.
Thanks…
Part Number: THS1206M-EVM Other Parts Discussed in Thread: TMS320F28335 , , THS1206
Tool/software: Code Composer Studio
THS1206M-EVM is connected to TMS320F28335,when D0-D11 are assigned to GPIO2-GPIO13 and CS1 /CS0 /WR /RD connect to GPIO68 70 72…
Hi Ash,
We have two enhanced versions of the THS1206, the THS1206-EP and the THS1206M. I don't see anything in our documentation that has them tested to any specific radiation levels.
Hi Wade,
Thanks a lot for the clarifications.
These parts are not visible on TI website so i was not able to confirm if they are TI or not.
I will create a separate thread for each of the components below:
5962-9762101QEA SN55LVDS31 5962-9754301QEA…
Hi Kiran,
Did you review the schematic in the THS1206M-EVM Users Guide? The connectors are identified there along with their pin functions. The THS1206 also has an input range of 2V, (from 1.5 to 3.5) so you'll need to level shift your input.
The…
Other Parts Discussed in Thread: THS1206 , THS1206M-EVM Dear Sir,
I have been facing same problem as Mr. Kiran in this post: http://e2e.ti.com/support/data_converters/precision_data_converters/f/73/t/236138.aspx
I gave a sinusoidal signal of 3V between…
Robin Lerche,
Robin: said: My question: Is it possible to use the ADC and DAC on the DSK6713? Is there any example-code?
Kindly have a look at the below wiki for DSK. It gives the software download link. http://processors.wiki.ti.com/index.php/C6713DSK_in_CCSv5…
Hello Mr. Thompson,
please use address 0xA0024000 with the jumper settings important to the address generation:
5/6K interface board (revB):
W1: open W6: 1-2
THS1206M-EVM
W2: closed W3: closed W4: A
If you have additional questions please…