Part Number: THS2630 Other Parts Discussed in Thread: THS4131 , Tool/software: Hello,
We have been using the THS4131 FDA is older designs and want to use the THS2630 going forward. We are using +/-15V supplies.
The simple LTSpice model here shows…
Part Number: THS2630 Other Parts Discussed in Thread: OPA1633 , OPA1632
I am looking for a single-ended to differential ADC driver.
The input is a single-ended signal span between -12 V & +12 V, frequency up to 25 MHz. I need to convert the +/-12…
Part Number: THS2630 Other Parts Discussed in Thread: TINA-TI Tool/software: Hi Experts,
Customer would like to use AMC3330QDWERQ1 which provide the isolation and output differential signal of 2V and at later stage I will use fully differential amplifier…
Part Number: THS2630
I was adding this new FDA to my parametric tables and noticed this common mistake, Rejection Ratio is a positive number, this is a plot of rejection,
Also, where is the Aol plot?
Part Number: THS2630
Hi TI team,
I am looking for a low-noise SE-to-Diff ADC driver to interface with the following parameter:
Input: +/-12 V span, single-ended
Output: +/-2.5 V differential across +2.5 V Vocm
The THS2630 seems the right…
Part Number: THS4532 Other Parts Discussed in Thread: THS2630 Tool/software: Hi team,
My customer's schematic is below. They want output offset as possible as equal to zero. Can some adjust method to improve? If change to THS2630, does the around component…
Part Number: THS4531 Other Parts Discussed in Thread: THS2630 Tool/software: Hi,
We're wondering if there is any specification for the common mode noise at the output of the THS4531 amplifier. Some amplifiers such as the THS2630 have it listed under…
Part Number: THS4131 Other Parts Discussed in Thread: THS2630 Tool/software: I am using Single ended to Differential opamp for this part number THS4131IDGNR, Vin = 3.3V, Vout = +/-15V I want Schematic for this part number THS4131IDGNR.
Part Number: THS4130 Other Parts Discussed in Thread: THS2630 Tool/software: Could you confirm that the marki ng in the picture is THS4130CDGK? Thank you very much!
Part Number: TMS320F28379D Other Parts Discussed in Thread: THS2630
Tool/software:
Dear Experts,
Hope everyone is doing fine!
Well, I am working on a project that requires high resolution ADC so using 16bit differential mode. The voltage levels…