Part Number: THS3001
Now the 30Mhz signal will have a gain that should not have been after this op amp, for example: the input signal is 30mhz amplitude 1Vpp, and the output of the simulation THS3001 is 1Vpp, but now the physical circuit output is 4Vpp…
Part Number: THS3001 Other Parts Discussed in Thread: THS3491 , LM7171 Dear Team,
Could you please tell us what is difference between THS3001HVIDGNR and THS3001IDGNR?
Also, Could you please tell us the latest version device of THS3001HVIDGNR?
…
Part Number: THS3001 Hi I'm sure Michael will have an answer to this one but I'm trying to get the very fastest settling time for the THS3001 when used at x2.5 and x4 gain. on the datasheet slew rate is quoted at x5 gain as 25-75% and is presumably much…
Part Number: THS3001 Hi,
I built a circuit based on a typical circuit, but the chip would burn as soon as it was powered on, which made me confused.
This is the schematic of THS3001.
Part Number: THS3001 Other Parts Discussed in Thread: THS3491 Hi, support team
My customer has the questions as follow:
I want to use THS3001 with single supply and output high voltage. But it didn't work. The gain is 2, using evaluation board.
…
Part Number: THS3001 Other Parts Discussed in Thread: THS3491 Hi I see from the datasheet that the DGN package has only 4.7 Degrees C/W thermal resistance to case. Is this the resistance to the thermal slug ? Also does anyone have the thermal resistance…
Part Number: THS3001 Other Parts Discussed in Thread: THS3491 Hi I saw Michael had posted in response to an earlier thread that this part wasn't recommended for new designs because of a resistor being too thin on the die. Yet when I look at the product…
Part Number: THS3001 Other Parts Discussed in Thread: THS3491 Hi I'm trying to do a thermal analysis and see typical input bias drift but can you let me know the worst case value ?
Thanks,
Steve
Part Number: THS3001 Other Parts Discussed in Thread: THS3491 , Hi teams,
THS3001HVIDGN gas two thermal pad packages like DGN0008D and DGN0008G.
Do we have any ways to specify the thermal pad package?
Best regards,
Shunsuke yamamoto
Proposed Thank you.
Will driving with one THS3001 put a strain on the device? (Does it lead to failure?) If it causes a failure, please tell me the conditions under which the device can be used without failure. (Output range that can guarantee device…