Part Number: THS4011 Hi,
I'd like to know if the THS4011 has ESD diodes tot he rails at the inputs and if so how much current can they handle?
Thanks,
---John
Part Number: THS4011 Hi,
I found the below statement in datasheet of THS4011.
Need help in understanding how the input offset voltage decreases with increasing frequency.
For THS4011, will the offset voltage reduce to uV range at what range…
Part Number: THS4011 Dear Community,
I would like to know what is the MM (ESD Machine Model) which this Op Amp withstand at while input is E2?
See the following attached picture:
Best Regards
Hi Ryuji,
The THS4011 thermal pad is electrically isolated from all terminals in the package. So, yes. It's power pad can be left floating. Do you know what OPA211A package is being used by the customer? The THS4011 SOIC (D) package does not have a…
Part Number: OPA847 Other Parts Discussed in Thread: THS4011 , THS4021 , LM311 , LM211 , LM111 , TLV3501 , TLV3601 The OPA847 part has absolute power supply range +/-6.5V and recommended range is +/-5V.
Do you have any similar part with higher voltage…
Hi Jacob,
I need a help regarding the composite opamp youi suggested to meet both low precision and high speed.
I tried to use a less precision opamp OPA627 followed by the fastest opamp THS4011 as shown below.
I find there are ringing at the output…
Part Number: THS4012 Other Parts Discussed in Thread: THS4032 , OPA2690 , OPA2691 , THS4011 , TINA-TI , OPA690 Hi Team,
I have created an 4 channel double isolation for analog video signal (CVBS). After optoisolation I have a video signal 1Vp-p with…
Duke of DACs,
I am driving my DAC8806 with an FPGA at 3.3v. Last week a GPIO pin on the FPGA quit working. It is connected directly to pin28(reset) on the DAC8806. I thought nothing of it as the FPGA has gone through a year of testing. I replaced the…
Part Number: DAC8806 I am driving my DAC8806 with an FPGA at 3.3v. Last week a GPIO pin on the FPGA quit working. It is connected directly to pin28(reset) on the DAC8806 . I thought nothing of it as the FPGA has gone through a year of testing. I replaced…
Hi Ryuji-san,
My apologies for the delay. As I had mentioned earlier, the EVM is mainly designed for DC performance evaluation and hence, it is not a godd idea to test settling time in a similar circuit. In case you have used OPA211 in your circuit…