Part Number: DAC8822 Other Parts Discussed in Thread: THS4011 Dear expert,
Here is a question about the "settling time" of DAC8822 vs. AD5547.
1, From the datasheet, we can see both DAC8822 and AD5547 have the same spec - 0.5us settling time…
Part Number: DAC7811 Other Parts Discussed in Thread: LM7705 , REF5050 , OPA376 , OPA727 , DAC8811 , THS4011 , LM4050-N-Q1 I need a 0 to 5V output from the DAC7811. I figured out a solution that I think will work, but I would appreciate it if someone would…
Kristoffer Flores said:
Brian,
I am actually surprised you are measuring THD levels that good... You are hitting the slew rate limit of the THS4011. The THS4011 has a listed slew rate of 310V/us with +/-15V supplies. Slew rate is the maximum rate of…
Other Parts Discussed in Thread: THS4011 Dear sir:
I got an application problem when designing my sallen key filter. I want to make filter bands adjustable through switching the capacitors
as attached. I plan to switch S1, S3 together in lower band…
Brandon,
Approach #1 is the cleanest.
I would recommend the THS4031 used in difference amp circuit. It uses similar internal architecture, except being single ended output, and is manufactured in the same process. It also has similar noise performance…
While I am waiting, I should mention that my present design uses the THS4211 instead of the THS3001, THS4001 or THS4011. So far, the THS4211 seems to compare well in terms of cost and capabilities, but I am open to suggestions if changes to the circuit…