Part Number: THS4304 Hello E2E,
I am hoping you can clarify some confusion I have on the THS4304 datasheet.
On the slew rate spec on page 6, it appears that there are the same parameters with different results. One is listed as 675V/us and the other is…
Part Number: THS4304 Hello,
The datasheet for THS4304 states that the absolute maximum input voltage is +/- Vs. Yet, under the Recommended Operating Conditions, the Input Common Mode voltage range extends beyond Vs +/-. So, what is the absolute maximum…
Part Number: THS4304 Hi,
Can you please confirm the peak to peak output swing for the THS4304 amp with split +/-2.5V supplies? Looks like only the single supply swing is given in the datasheet
Thanks,
Anoop
Part Number: THS4304 Hello I've encountered myself with a board that uses a THS4304 as a unity gain buffer, and some components had to be changed (same value of components, just different lot) and the circuit started to oscillate around 900MHz to 1GHz…
Part Number: THS4304 Other Parts Discussed in Thread: OPA693 , , THS4302 Dear experts,
Customer is looking for high speed amp to replace OPA693(Gain =2) which is used for 130MHz clock .
Must Requirement :
Supply : 3.3V, Package thickness : 1.3mm under..
…
Dear Loren
Thank you for your reply.
I am still considering the difference.
THS4304 is selected tentatively, it can be changed.
In this case, do you have any recommend device?
On the other hand, I confirmed low pass filter and high pass filter, there…
Other Parts Discussed in Thread: THS4304 I'm trying to use the Hamamatsu G8931-04 APD with the THS4304.
I have the eval board and using the inverting input at the Gain 1.
I am operating the APD at or near breakdown.
The 4304 seems to be loading the…
Part Number: THS4302 Other Parts Discussed in Thread: THS4303 , THS4304 , , TL081 , LMH6521 , LMH6523 , LMH6554 , LMH2832 , LMH6881 , OPA857 , TINA-TI , BUF802 Hello there,
I am willing to buy THS4302, THS4303, THS4304 op-amps. I came across with few problems listed…
Other Parts Discussed in Thread: THS4304 , TINA-TI , THS4302 We used TINA-ti simulation the THS4304 USB D+ signal enlarge application. Please refer to the below circuit & wavefrom. The signal enlarge signal twice. Why we test the THS4304 circuit output…