Ryan, I believe the confusion is on my end. I have gone back to both datasheets and I did misunderstand the FSR of the ADS1278. I thought the FSR of +/-Vref was midscale plus/minus Vref, which in my case would have been a 0V to 5V input. My gain setting…
Part Number: THS4524EVM Other Parts Discussed in Thread: THS4524 , THS4521 , , ADS1278-EP Hello, I am reviewing the THS4524 datasheet to the THS4524EVM schematics and I have a question. The first picture below is from the datasheet for the THS4524 and the…
Part Number: THS4521 Other Parts Discussed in Thread: THS4524 , THS4522 , , TINA-TI , LMH6554 , LMH6552
Hi team,
The customer would like to use THS4521,THS4522 and THS4524. He needs to know the delay time of these devices that is the time for the signal
from…
Hi,
I used THS4524. After changes you mentioned new pcb are still broken. I will send you full design in private message, but you can answer here so maybe it will help other users :)
Part Number: ADS1174 Other Parts Discussed in Thread: THS4524 Hello, I am carrying out current measurements using Rogowski coils, one Operational amplifier THS4524, and one ADC ADS1174. When installed, the device is working 24/7 without interruption. Few…
Part Number: ADS1278 Other Parts Discussed in Thread: THS4524 , OPA2350 Hi,
I have a situation with the ADS1278 where it is likely that the /PWDN pins could be active at 3.3V, and only the 1.8V and 3.3V rails are active. The
3.3V /PWDNx voltage is created…
Part Number: THS4524EVM Other Parts Discussed in Thread: THS4541 , THS4524 , TINA-TI , THS4521 Hello, I am looking for a solution to add (or subtract, same thing) up to 4 RF frequencies, and I am wondering if THS4524EVM is a good candidates? Would it be…
Other Parts Discussed in Thread: THS4531 , THS4531A , THS4524 , THS4522 , THS4521 I think there are errors in the spice models for the THS4531, the THS4531A and TH4532.
The THS4531.TSC example (in EXAMPLES\TI Test Circuits) yields an operating current of almost…
Other Parts Discussed in Thread: ADS1248 , THS4524 I have to measure strain (quarter bridge three wire), using 350ohm and 1K. Problem is signal change is so small . I have attached the circuit. I am using internal IDAC of ADS1248. 1. For 1K strain , voltage…