The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.
Other Parts Discussed in Thread: THS4524 , ADS1274 , OPA2365 , TPS717 Hello,
on a board I am using a TPS71750 (DSE type) in order to power: ADS1274 (75 mA max in high resolution mode), THS4524 (5.2 mA max), OPA2365 (10 mA max) and three accelerometers (10…
Other Parts Discussed in Thread: THS4524 , THS4521 , PCM4204 , THS4509 , TINA-TI Hi!
I have some questions regarding the THS4524 opamp.
I plan to use a single +5VDC supply for the opamp. The input signals are differential (symmetrical) signals with a common…
The problem with rolling your own version of the first half of the instrumentation a amplifier is the cost of the accurate resistors. Otherwise it wouldn't be a problem.
I have a low impedance sensor (375 ohm nominal) that needs around 1500ohm damping…
Other Parts Discussed in Thread: THS4130 , ADS1278 , THS4524 , THS4522 , THS4521 Hello,
I need to design an fully differential ADC driver that can handle a +/-15V input signal. I was looking at the THS4130 as an option. I need the design to be as low power…
Other Parts Discussed in Thread: THS4522 , THS4524 6406.THS4522 - PCB schematic.pdf 4061.ths4521 TINA.pdf
Hi,
my problem is that the Tina 's simulation working well , while in the real circuitry I have DC voltages that should not be there .
The dc voltages in the nets…
Todd,
On the input filters, capacitors such as C209 (0.047uF) are hooked up to both outputs of the THS4524 devices. When connected this way, the capacitor's center is rotating around the common - mode, and this results in the capacitor's value effectively…
TI just introduced the THS4521 (single), THS4522 (dual), and THS4524 (quad) family of low power, high performance fully differential amplifiers that are targeted at driving SAR and Delta-Sigma ADCs in many applications including audio. Its performance…
Other Parts Discussed in Thread: ADS8412 , ADS8318 , THS4520 , THS4521 , THS4131 , THS4524 , THS4522 , THS4509 Sir,
I have differential Inputs
VS - 2 to 2.7V
VR - 2 to 1.3V
I want to design ADC Card with differential amplifiler.for 14/16 bit ADC
can you suggest…
Other Parts Discussed in Thread: ADS1278 , THS4521 , LMH6551 hello
I am trying to use THS4521 with ADS1278 with vcom coming from adc as 2.5V.
Supply given for FDA is Vs+=5V and Vs-=GND, for ADC is AVDD = +5V
The analog input voltage is +/- 5V, with Vcom =…
Other Parts Discussed in Thread: THS4521 , TINA-TI Hello!
I have an application which requires conversion from a single-ended input to a differential output for a high-precision ADC. I only have access to a +5V source, so my initial design was as follows…