Part Number: THS4631
Dear Experts,
I have assembled the peak detector circuit using THS4631 as shown below. https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/940064/how-to-improve-the-accuracy-of-peak-detector-as-high-as-posssible#pi320995…
Part Number: THS4631 Other Parts Discussed in Thread: OPA656 , OPA810
My question is, does TI have a curve or data shown the input current noise density as a function of frequency for frequencies above 10 kHz, extending up into about 1 MHz?
For some…
Part Number: THS4631 Tool/software: Hi,
I am using the THS4631 in a high-voltage differential measurement probe where I need to measure an analog signal with a frequency up to 50MHz. A 49.9-ohm resistor is connected between the op-amp's output and the…
Part Number: THS4631 a. Is there a protective diode built in between the input terminals of the THS4631?
b. If it is built in, can you tell me the current-voltage characteristic and the conditions under which it is used?
For example, as follows, …
Part Number: THS4631 Other Parts Discussed in Thread: THS3491 , , OPA548
Hello!
I always thanks for your great supports.
Back in the last thread, I solved problem to reduce the cable and improve Rf 30 to 800ohm. (Thanks Kai )
But unfortunately…
Part Number: THS4631 Dear TI expert,
I wonder for THS4631, if I can connect its pin 1 to Ground, pin 8 to VS+ (i.e., pin 7)? The datasheet says they are NC pins, and I'm not sure if connecting them to ground or positive supply will be ok?
Best…
Part Number: THS4631 Other Parts Discussed in Thread: TINA-TI , , OPA320 , LMP7718 , OPA838 Hello,
I connected the DUT to the network analyzer (Agilent 4395A). The configuration is shown below.
The bodeplot of the DUT, connected to the VNA, is shown…