Part Number: THS6214 Other Parts Discussed in Thread: THS6204 , , THS6062 , THS7002 , THS6002 , THS6301 , THS6302 , THS6222 , THS4561 , THS4551 , THS4541 , OPA2863A , OPA863 , OPA2863 , OPA810 Hi TI Team,
I search the receiver that can match with THS6214…
Thanks,
1. my chip is damaged。 so I can show the signal wave by my hands only.The input signal is 3MHz Sin wave.
In my views,The output discontinuity is due to chip overcurrent protection or overheat protection.
2. The R100 and R114 has been…
Part Number: THS6214 Hi Team,
My customer is using THS6214/2 in broad band PLC application. And now we have a concern about the D1/2 Out pins voltage tolerance.
In my design, Vs+ = 12V, Vs- = 0V. and we have a TVS diode connected from D1/2 out to…
Part Number: THS6214 I have 3 questions to ask, pls help to give some advise, many thanks!
1.In THS6214 application use 12V power supply, when the external 15V interference continued to interupt Pin D1OUT & D2OUT, it can be destroy the IC or what influence…
Part Number: THS6214 Hi Team,
I have tested TI THS6214, the power supply is 12V, and I found we have a 6V bias on Pin20 and Pin17, may i know the reason why we have a bias ? And what is the maximum voltage tolerance of Pin20 and Pin17? Any comments…
Part Number: THS6212 Other Parts Discussed in Thread: THS6214 Hi,
One of my customer met the problem when using the THS6212 and THS6214, and the problem shows as below:
THS6212 & THS6214 test waveform is compared as follows:
THS6212
THS6214…
Part Number: THS6214 Other Parts Discussed in Thread: DP83TC811 ①If the above-mentioned DSL line driver and PLC line driver are used, can the communication transmission task be completed?
②If the line driver can be used to accomplish the goal, can you…
Part Number: THS6214 Hi,
In table 1 of THS6214 datasheet, the BIAS pins are named as 'BIAS-1' and 'BIAS-0'. While the pin name is in fact 'BIAS-1' and 'BIAS-2'. Obviously this is a typo. How should i corresponding 'BIAS-1' 'BIAS-0' to pin name 'BIAS…
Other Parts Discussed in Thread: THS6214 For operating a THS6214 between +/-12V power and for maximum bandwidth, should Iadj be connected to ground, +12V or -12V and what is the resistor value ? I assume the Bias would be set to Full for the maximum bandwidth…