Other Parts Discussed in Thread: THS6226 Dear Sir,
I got a project for 4-port DPU design need your hlep.
1. Channel AB's SNR is better than Channel CD's. I need to get some suggestion from you.
- loop length = 0m, 200m, 250m.
2. For programming…
Other Parts Discussed in Thread: THS6226 please tell us how to treat the unused part/pin of ths6226 ?
for example, I can leave the part AB without power or better off via serial interface and leave pin floating? if I can leave it without power, as is…
Hello Ervin,
You will notice the the THS6212 and the THS6214 are marketed differently (one is PLC while the other is DSL) although they are essentially the same part with a different number of channels. Both parts can be used in either application.…
Class G and class H amplifiers are a approach to modulating the supply similar to an envelope tracking.
The THS6132 is a class G amplifier and will tarck teh signal automatically, but is limited to lower frequency range as the power supply of the amplifier…