RS-4xx devices are more power hungry and, in general, more expensive.
When using many channels, see, e.g., the AM26C31/AM26C32 or AM26LV31/AM26LV32; for the back channel, use any 1+1 transceiver like the THVD1500 or THVD1400.
Part Number: THVD1406 Other Parts Discussed in Thread: THVD1400 , Hi Team,
I understand that It is recommended that pull down /SHDN pin to GND through 10kohom.
However, our customer would like to pull up /SHDN pin to VCC=3.3V through 10kohm.
(So, they…
Other Parts Discussed in Thread: THVD1426 , THVD1406 , THVD1454 , THVD1420 , THVD1400 , THVD1410 Dear Experts,
Currently, i have used the below design for RS485 to TTL with auto flow control(74HC), now i have the plan to redesign my converter with ti RS485 converters…
Part Number: THVD1406 Hi Team,
We understand that your recommended ESD protection device is CDSOT23-SM712.
However, our customer would like to use Varistor(AVRM1608C270MTABB) for two connecters of daisy chain.
Could you please let us know if you know…
Below the minimum supply voltage of 4.5 V, correct operation is not guaranteed.
The description in table 3 is wrong; it was probably copied from the SN65HVD72 datasheet. Also consider the newer THVD1400/10.
Other Parts Discussed in Thread: ISO1500 , THVD1400 Dear Sir,
My customer has a question about the power consumption of RS485 while designing it.
Add pull high or pull low resistor will increase power consumption. If the Voc is 3.3V, then there will…
Part Number: THVD1551 Other Parts Discussed in Thread: THVD1552 , , THVD1505 , THVD1400 , THVD1520 , THVD1420 Hi there,
I would like to use 5V SSI transceiver for my motor control application. I would like to use single channel version of ADM4168E from ti…
Part Number: SN65LBC184 Other Parts Discussed in Thread: THVD1410 , , THVD1500 , THVD1510 , THVD1400 Hi,
Good Day. Can the customer use SN65LBC184 as a replacement for the MAXIM part MAX483ECPA+. As I check the BOM and cross reference tool, SN65LBC184 is not…
Other Parts Discussed in Thread: THVD1429 , THVD1450 , SN65HVD70 , THVD1420 , THVD1426 , THVD1449 , THVD1400 Hi, Kindly Suggest the Alternate Part's (Direct Replacement) for ST3485EIDT (ST Microelectronis), without design/footprint modification. Because this…
Other Parts Discussed in Thread: SN65ALS176 , THVD1505 , THVD1400 Hi everyone,
SN65ALS176 is declared to work properly between 4.75V and 5.25V
If I suplly the transceiver with a power supply of 4.5-5.5V, what kind of malfunction or degradation should I observe…