Part Number: THVD2450 Hi,
A recent batch of THVD2450DR parts we received are marked with a date/location code of 12M, inconsistent with all the earlier parts received which had codes ending in K.
Given that the "Quality, reliability & packaging data download…
Hi Eric
The following is the transmission waveform of sn65hvd485e (connect the GND of sn65hvd485e to the GND of the probe):
The following is a transmission waveform thvd2450 (GND thvd2450 access probe to the GND):
The cable length of RS485 is 60c…
Part Number: THVD2450 Hi, We want to use the THVD2450 in one of our project. Pulse skew is a critical parameter in this application. Does TI has any figure that shows typical Pulse skew vs Temperature charateristics? Does MAX value include full temperature…
Part Number: THVD2450 Hi, We plan to use the THDV2450 because of its robustness and the extended operational common mode range. Now I have seen that there are three packages available but none of them have stock. The only one that is available so far is…
Part Number: THVD2450 Hi,
To save space and upgrade robustness against machine wiring faults, I am considering upgrading from
SN65HVD485EDR (in SOIC8)
to
THVD2450 (in VSSOP8)
in this new version of the circuit board.
Is THVD2450 the best choice for industrial…
Part Number: THVD2450 Tool/software: WEBENCH® Design Tools Can I use CPDQR24V-HF instead of SMAJ30CA? We need a TVS with the same package size as CPDQR24V-HF. Do you have a better recommendation?
Part Number: THVD2450
It is about suitability of very universal THVD2450D use in configuration with one termination resistor 470R at the receiver (This is to limit the current drawn by the transceiver line).
We want to use this RS485 transceiver only…
Part Number: THVD2450 Hello Guys,
Good day.
Our customer wanted to know if the driver output current (IO) specified as –60 to 60 mA on the datasheet of THVD2450 is an RMS value?
Thanks to confirm!
Art
Hi Eric,
AM26C31(TX) for the outputs and either THVD1450 or possibly THVD2450 for the (RX) are probably the best suited 5V supply devices for this type of application with the fewest number of IC's. For 3.3V supplies AM26LV32E is a good device.
…
Part Number: THVD2450 Hi,
i've got a question regarding the direct connection of the driver enable pin "DE" and the receiver enable pin "RE", which is active low. I'm planning to short these pins together, when connecting them to…