Part Number: THVD8000 Other Parts Discussed in Thread: THVD8010 Tool/software: Hi
AC line PLC communication is being implemented using THVD8000
1. Problem: Noise is recognized as carrier when communicating using AC line and the UART bit is broken (see…
Part Number: THVD8000 Other Parts Discussed in Thread: TCAN330 , THVD8010 , THS6222 Tool/software: Hi team,
I have a question about THVD8000, could it work with CAN communication?
BR
Jingguo
Part Number: THVD8000 Tool/software: Hello!
We are working on an application were the power line must be a square or sinusoidal wave between 50KHz to 100KHz (under development yet), that is then rectified in the receiver to supply a DC load of 10V 1A…
Part Number: THVD8000 Tool/software: Hi,
The design requirements for a Fire Panel system, demand power line communication over a distance of more than 1.2 km.
More than 254 devices (detectors) would be interfaced to the main control panel.
Suggest possible…
Part Number: THVD8000 Tool/software: Hi,TI Engineer
Can I use a common mode inductor to replace the two inductors(L1,L2) (L3,L4) here,To reduce PCB area。
Part Number: THVD8000
With the THVD8000 transceiver, what should be the observed behavior for bus contention? Are the observations deterministic for all combinations of dominant and recessive bit collisions?
Part Number: THVD8000 Hi team,
we are seeing the MODE signal of THVD8000 is off for about 2us, there is a probability of outputting a 0.5us low-level pulse from the R pin. Is there any possibility to cause this pulse?
Green is MODE, purple is R
Part Number: THVD8000 Hi team,
my customer target to use 3V3 MCU to communicate with THVD8000, but we are seeing the Vod parameter is under 5VCC level and then it can get enough Vod magnitude.
meanwhile ,the VIH >2V is okay for 3V3 MCU, but VOH =VCC …
Hi Marc,
No problem - I am not sure why they put that in the text - I understand the confusion.
Common mode chokes are used in THVD8000 applications (or power over bus - but generally THVD8000 is better than standard RS-485 over bus) - but more for common…