Part Number: THVD8000 Other Parts Discussed in Thread: TCAN330 , THVD8010 , THS6222 Tool/software: Hi team,
I have a question about THVD8000, could it work with CAN communication?
BR
Jingguo
Part Number: THVD8000 Other Parts Discussed in Thread: THVD8010 , , THS6222 Hi,
Really interested in the THVD8000 & THVD8010 devices, do you think they would be suitable for a low data rate application on industrial vehicles, like an electric forklift truck…
Part Number: SN65HVD1787 Other Parts Discussed in Thread: TIDA-00527 , THVD8000EVM , THVD8010 , THVD8000 We are a company that designs lighting dimming control boards from south Korea.
We would like to control lighting dimming using PLC IC (SN65HVD1787) …
Part Number: SN65HVD23 Other Parts Discussed in Thread: THVD8000 , , THVD8010 Hi,
We have requirement for RS485 power over communication with data rate 10Mbps upto 500m cable distance. It is noted that the THVD8000 device can be used with two-wire cable…
Answer for your questions:
1. Schematic if possible - it looks like there is noise on the bus and that can originate from an unoptimized schematic.
2. How many THVD8000 Nodes are in the system? → 1 on 1 systems
3. What is the length of the bus from…
Part Number: THVD8000 Other Parts Discussed in Thread: THVD8010 , In my opinion, if 0.1uFs are connected in series 2EA, it becomes 50nF, so isn't the impedance Z going to be 6.36 ohms?
---------------------------------------------------------------…
Part Number: THVD1406 Other Parts Discussed in Thread: THVD8000 , THVD8010 Please see attached file.
Is it possible to use the THVD1406 to communicate a signal with a DC power supply?
Please let me know if you have any problems.
I know THVD8000 RS-485…
Hi Jacky,
Thanks for reaching out!
1. At 1km @ 19.2kbps (minimum OOK modulation for +/- 2% duty cycle distortion is 192KHz - closest available modulation frequencies are 187.5KHz (which could cause more duty cycle distortion ) and then it goes to 500KHz…
Hi Rayna,
A few comments on the schematic - as anti-interference also is going to require a larger SNR - which means you cannot overload the bus - this design is overloading the bus.
C19 and C20 alone violate common mode loading of THVD8000 - at 2MHz…