Hello
Please help to see if Ti has any recommendations to replace MP3425DL
Boost chip IC-Boost DC-DC Controller Boost,24V/3.5A,1MHz,Fb1.35V,14-pin QFN,3*4*0.9 Original model:MP3425DL
MP3425DL.pdf
I am currently using several Enpirion switching regulators and power modules in my designs. However, it was recently announced that Intel will be obsoleting this entire portfolio. Does TI have crosses for these Enpirion devices?
Hi team,
Does TI have a suitable DC/DC solution to MIC33M350 or MIC24046? thanks!
Vin=5V
Vo=1.2,1.5V,1.8V,2.5V,3.3V
Io=1A
feature :Output voltage pin selectable
Part Number: TI-PLC-PRIME-DC Other Parts Discussed in Thread: AM3356
Can the upper level prime-dc v4.0.0.0 binary run on AM57x family with out an issue? Does it need to be recompiled for AM57x Family?
The below link describes that the upper levels of…
Part Number: LM5023 Other Parts Discussed in Thread: TPS92314 , UCC28056 , UCC28051 , UCC28050
Hii Everyone
I am using the LM5023 PWM controller for the design of a 19 V, 60 W AC-DC converter. For this design, how can we improve its power factor?
Thanks…
Part Number: LM5021 Hii Everyone
I am using the LM5021 PWM controller for the design of a 24 V, 90 W AC-DC converter. What is the purpose of using Zener diode (Dreg) and capacitor (Creg) used in voltage divider circuits?
Thanks and Regards
Abhishek
Part Number: UCC2803 Other Parts Discussed in Thread: TINA-TI Hii..
I am designing an AC/DC converter of 60 W, 19 V output but after simulation in Tina-TI using UCC2803, the pwm controller is turning on, but not getting output voltage. What to do?
Attaching…
Part Number: UCC2803 Hii Everyone..
I am designing a 19 V, 60 W, AC-DC flyback isolated converter using UCC2803 Controller, but I am facing an issue in the voltage divider circuit on the secondary side. As suggested in the Webench design there should…
Part Number: UCC2803 Hii Everyone,
Using UCC2803, I am designing a 60 w, 19 V ac/dc converter. The PWM controller is turning on, but not getting proper output voltage.
Attaching circuit design of Webench, my own simulation, and its waveform.
Please R…
Part Number: TI-PLC-G3-DC
Hi,
I repost this thread as another thread end up with no reply. Some one told me I would see something back from him Monday or Tuesday at the latest. I keep waiting but so far I didn't get anything.
Who can tell me if there…