Part Number: TIC10024-Q1 Dears:
At present, Customer has found that part of the channel level acquisition failure of TIC10024QDCPRQ1 chip in product fault analysis, and the relevant situation is described as follows:
1. Recently, the end customer has…
Part Number: TIC10024-Q1 Hi Team,
One of my KMM asked for direct support of their issues instead of Arrow support. They are having an issue related to TIC10024-Q1. Please help me support them. Below are the questions.
They want us to go over SPI waveform…
Part Number: TIC10024-Q1 Hi Expert,
For TIC10024-Q1, does it have hysteresis function for inputs signals? I don't read related in datasheet. I think it should have. Could you please help to verify? Thanks.
BR,
Elec Cheng
Part Number: TIC10024-Q1 Hi team,
In which condition does it need external ESD protection circuit?
Datasheet "Figure 10-1. Using TIC10024-Q1 to Monitor a Digital Switch in Body Control Module Application" includes external ESD circuit RESD and CESD. But…
Part Number: TIC10024-Q1 Hi team,
Datasheet shows "Figure 8-13. Example For Ignored Switch Position Change Between 2 Wetting Current Cycles", could each lower case handle switch state change reflecting in SCC bit in INT_STAT and IN_STAT_COMP register…
Part Number: TIC10024-Q1 Other Parts Discussed in Thread: TIC12400-Q1 , Hi team,
I have a question about the configuration of the TIC10024-Q1(or TIC12400-Q1).
1. Wetting current.
I want to control the wetting current strictly between min 5mA max 10mA,…
Part Number: TIC10024-Q1 Other Parts Discussed in Thread: TIC12400-Q1 Dear team,
This is Chris from TI Korea and one of my customers is going through an error that happened during ESD test with the switching IC. I explained in detail about the current…
Part Number: TIC10024-Q1 Dear team,
Does our comparator threshold have hysteresis? For example, we choose THRES_COMP=2V, if the input signal varies from 1.9V to 2.1V, then the result will change, right? If we don't have hysteresis, our device will have…
Part Number: TIC10024-Q1 Other Parts Discussed in Thread: TIC12400 Hi Expert,
Our customer develop a set of software programming for TIC12400. And now they wants to use the same programming for TIC10024. Since TIC12400 has more function than TIC10024, so they…