Part Number: TIC12400-Q1 Other Parts Discussed in Thread: TIC10024-Q1
Hi, Support Team
We would use TIC12400-Q1 to replace NXP MC33CD1020AES.
we have few question as below list:
Q1: in polling mode, only IN PIN status to change to wake up MSDI? Could…
Part Number: TIC12400-Q1 Other Parts Discussed in Thread: TIC12400 , Hello team,
We use IN0 and IN1 of TIC12400 as CAN interrupt wake-up detection. Due to the leakage current in INx and the large external resistance added to IN0 and IN1, when the MCU goes…
Hi Jonathan,
Thanks for connecting through mail. Further to our discussion. can you please address following our query
In the process of diagnostics/automotive safety considerations, whether Inx pins of TIC12400-Q1 are designed for detecting of short…
Part Number: TIC12400-Q1 Other Parts Discussed in Thread: TIC12400 I use the TIC12400 for monitoring individual relays (no matrix arrangement!).
I have configured the TIC12400 pins IN0 as "Sink" and IN10 as "Source". I want to use…
Part Number: TIC12400-Q1 Other Parts Discussed in Thread: TIC12400 Hi TI team,
I am working on interfacing TIC12400 with the microcontroller using SPI and configuring the required registers. Whether any sample code is available for that. Kindly help me…
Part Number: TIC12400-Q1 Other Parts Discussed in Thread: TIC12400 Hi,
In TIC12400, I came to know from the datasheet that the input pins can be configured into two modes. ADC or comparator. But in input channels IN0 to IN11 there are only one threshold…
Part Number: TIC12400-Q1 Other Parts Discussed in Thread: TIC12400 , Hi Team,
The requirement for the resistor coded switch to be interfaced with the MSDI is as follows:
10K when switch not pressed
Press to Ground when the switch is active.
and the wetting…
Part Number: TIC12400-Q1 Other Parts Discussed in Thread: TCAN1145-Q1 Hello team,
Can you help confirm what is the internal block diagram of SPI signal inside the TIC12400-Q1?
Four signals: CS, SCLK, SDI,SDO, how do they connect each? pull up resistor to…
Part Number: TIC12400-Q1 Hello experts,
I saw there is a RIN,SC input resistance=240kOhm on the page 8 of the datasheet. I suppose this is a pull down resistance right? Should we consider this resistance when we doing the ADC sampling accuracy calculation…