I looked at the firmware section of TIDA-00069 and all I found is a binary QAR file.
Can you provide a text file of the source code?
QAR is for QUartus (Altera) which does not work fo rXilinx FPGAs.
Sajad,
An example firmware doing this has been done as a TI-Design TIDA-00069. However this is a custom firmware and will not work with HSDC Pro as the normal firmware does - it only implements a basic FIFO from ADC input to DAC outupt. If you want…
Hi,
I think you would want to ask your FPGS vendor for the recommended FPGA development platform to use.
we have been using the 2-segment Samtec connector on our LVDS ADC EVMs for many years now, with a pinout we defined to work with the capture cards…
Yes - you may use the TSW1400 as an FPGA platform. However we cannot support any custom firmware - you will need to work with Altera if you run into any problems.
There is a JTAG port on the TSW1400 if you wish to use Quartus and treat the TSW1400 as…
Part Number: ADS4249 Other Parts Discussed in Thread: 4213 In reply to FRK :
Dear
Can you please suggest me any Xilinx IP core compatible with Altera Megafunction ALTLVDS_RX and ALTPLL. I am configuring ADS4249 with Xilinx VC 707 kit. After going through …
Samet,
Have a look here. This outlines an example of how to do this. The DAC is different but you can use this as a starting example.
www.ti.com/.../TIDA-00069
Ken.
Hi,
The TSW1400 capture card uses an Altera FPGA to capture data from the ADS5463 EVM as well as many others, and the Altera Quartus project files are available for download from the TSW1400 page at http://www.ti.com/tool/TSW1400EVM?keyMatch=tsw1400&tisearch…
Other Parts Discussed in Thread: DAC5682Z , TIDA-00069 TSW3100 FPGA data(VHDI etc) of Stratix II
Hi,
My customer is using DAC5682z. He wants the reference design of FPGA soft. Especially, the reference design of part of connecting with DAC.
Could TI provide…