Hi,
hopefully the TIDA-00129 Test Results Section Description can already help you to get started here.
It gives some indications what to modify.
Is that what you indicate with "modify TIDA-00120 design"?
Thanks,
Britta
Dear Sahitya-san,
I think you found an error in our user guide. It has the wrong formula at this place. Because I'm not the author of the guide I'd need some time to work on the correct formula.
In the mean time please have a look at following TI…
Hi Mansur,
A boost converter with integrated FET can be used to get from 12VDC to 24VDC. Examples are LM5001 and TPS71175 for the given output current of min 400mA. This are non-isolated solutions.
If you need channel-to-channel isolated solution…
Other Parts Discussed in Thread: TIDA-00129 , LM5017 Hi,
I am supporitng industrial customer in Japan, customer needs isolated 26V/30mA and 5V/20mA from Vin 24V which ranges 20.8V to 28.8V.
I am considering using TIDA-00129 which is similar design…
Dear Gaurang,
Thank you for evaluating this power design.
The isolation depends exclusively on the PCB parameters. These are given by your own PCB design and by the physical dimensions of the coil. To support your requirements you can remove the negative…
Hello Diogo,
Unfortunately our expertise in this forum is not in the design of power supply circuitry for the DAC devices but rather the functionality and performance of the DAC devices.
That said, the TI PowerLab provides an easy way for you to design…
Hello Onur,
I attached the application notes and a tool to help you select and design solution for flybuck application for your operating conditions:
7462.slpc017b.zip
how to design fly-buck.pdf
Pick the right turns ratio for flybuck.pdf
Flybuck…