Part Number: TIDA-00218 Hello. I am wondering if the firmware files are provided for TIDA-00218. There is a section in the user manual regarding explaining firmware features, but the design folder does not include any firmware packages. Is there a way…
Part Number: DRV5053 Other Parts Discussed in Thread: TIDA-00218 Hi, in the TIDA-00218 design, we mentioned "Contactless Proximity Current Sensing for AC, 3-Phase Input Currents".
And a customer is asking how we measure the AC, 3 phase input currents…
Hi Javier,
TIDA-00218 is used to measure AC current, can it measure DC current up to 800A? Do you have any app-notes on this application?
Thanks very much!
Hi Suneetha, we do have this TI Design, which uses a flux concentrator around a cable: http://www.ti.com/tool/TIDA-00218
Is there a certain bandwidth you need?
Best regards, RE
Yes, and here is a reference design: http://www.ti.com/tool/TIDA-00218
The max current sensed depends on the flux concentrator used, the air gap, and the distance to the wire.
The DRV411 is more specifically targeted at current sensing, and can give…