Part Number: TIDA-00254 Other Parts Discussed in Thread: DLPLCR4500EVM Hello!
I am using the reference design TIDA-00254, with DLPLCR4500EVM.
I can set the led current value to all 255 with DLPLCR4500GUI-3.1.0 and no problem.
When using the reference…
Part Number: DLPLCR4500EVM Other Parts Discussed in Thread: TIDA-00254 , Hello!
I am using the reference design TIDA-00254, with DLPLCR4500EVM.
I can set the led current value to all 255 with DLPLCR4500GUI-3.1.0 and no problem.
When using the reference…
Part Number: TIDA-00254 The reference design supply the cameras that can be used, which is point grey FlyCapture2 or Microsoft LifeCam Cinema.
Can I use other cameras instead of the two above cameras?
If the camera can be replaced, what's the requirements…
Hello Mr. Vivek,
Thank you so much for the detailed information.
Just one more query.
The TIDA-00254 Test Results shows use of a DLP® LightCrafter 4500 EVM for point cloud generation.
Just wanted to know if the software used for the same (i.e. the .exe…
Part Number: TIDA-00254 Other Parts Discussed in Thread: DLP4500NIR , , DLP4500 I saw that there is a NIR version of the DLP4500 DMD. Does the TIDA-00254 reference design also work with the DLP4500NIR DMD? Is it possible to replace the DMD or purchase the…
Part Number: TIDA-00254 Other Parts Discussed in Thread: DLPLCR4500EVM , Hi,
When I doing the step 2, I got the Error as follow:
LCR4500_DEBUG<0X28ef08>: Flash device parameters NOT found
Projector prepare sequence FAILED:
ERRORS: 1 and WARNINGS:…
Part Number: TIDA-00254 Hello ,
I am using Dlp lightcrafter 4500 with a point grey camera, i need some help to resolve my problem. I completed my setup following the user Guide and completed until calibration of camera and system.
When I try to scan for vertical…
Part Number: DLPLCR4500EVM Other Parts Discussed in Thread: TIDA-00254 Hello,
Does anyone have example C++ or Python (using pycrafter4500 library) code demonstrating how to project patterns to the LCR4500 via USB?
I am having some trouble figuring out…
Part Number: DLP4500 Other Parts Discussed in Thread: TIDA-00254 hi, I am using tida-00254's user guide in step 3.6-> 5. Enter menu option "4"...
But the error message shows "Camera NOT connected!"
But when I use camera_view_opencv…
Part Number: DLP4500 Other Parts Discussed in Thread: TIDA-00254 hi, I am read TIDA-00254's user's guide.
In step 3.5 after entering 1.
It show error CALIBRATION_PARAMETERS_MODEL/IMAGE_SIZE_MISSING.
How can I fix it?
Thanks for the reply!