Hello Munseong,
munseong kong said: I want to make solenoid current to 0A when EN signal is Low. And the Gate Signal from DRV110(OUT) is Low.
When EN is LOW, the output is disabled and current will be ~0A. There can be some leakage current making…
Part Number: TIDA-00289 Other Parts Discussed in Thread: TIOL111 , TIDA-01250 Hallo TI's team, I am looking for a solenoid control solution with the following parameters: Voltage: DC3V Power : 8W Current: 2.68A Resistance: 1.12Ω Working Cycle: 0.5s On…
Part Number: TIDA-00289 Other Parts Discussed in Thread: DRV110 , TPS272C45 Hi all.
I need to design a new board in order to replace the original drivers for some HVAC's fluid control valves operating in the 0-20V DC range in phase cut mode. The steering…
Part Number: TIDA-00289 Other Parts Discussed in Thread: DRV110 , DRV5023 , OPA4170 , , TLV271 The TIDA-00289 design uses a 24-V DC solenoid, can the design be easily modified for 12-V DC solenoids? I checked the datasheets for the major components (DRV110…
Part Number: TIDA-00289 Other Parts Discussed in Thread: TIDA-00284 Hi,
I need to design a plunger movement detection for elevator brakes in which the DC voltage used to excite the coil is always unfiltered DC and comes directly from a bridge rectifier…
Part Number: TIDA-00289 Hi,
I need to design a plunger movement detection for elevator brakes in which the DC voltage used to excite the coil is always unfiltered DC and comes directly from a bridge rectifier. In this reference design the used voltage…
Part Number: TIDA-00289 Other Parts Discussed in Thread: DRV110 ,
What is the max voltage of DRV110 EN and STATUS pins? Spec sheet seems to say 7V but in TIDA-00289 the STATUS pin is tied up to VIN=15V which is a lot more convenient in my design.
Part Number: DRV110 Other Parts Discussed in Thread: TIDA-00289 , INA250 Hello
Just ordered some DRV110APWR and I intend to control a 10 Ampere (peak) solenoid using TIDA-00289 guidelines and a BUZ11 mosfet. The solenoid will drive a clutch.
Do you…
Part Number: TIDA-00289 Other Parts Discussed in Thread: DRV110 I have a question regarding the latch in TIDA-00289, specifically how the plunger movement detection circuit resets.
Much treatment is given to the operation of the plunger detection circuit…