Dear Armen,
The details of DLP2010 EVM are available as TI reference design (TIDA-00325).
www.ti.com/.../tida-00325
Hopefully, this reference design can provide information you are looking for.
Regards,
Vivek
Briens,
Based on the schematic for this EVM (from https://www.ti.com/tool/TIDA-00325 ) D5 is HOST_IRQ, D6 is RESETZ, and D9 is one of the MSP430 status bits (for use during communication).
If HOST_IRQ is not going low and RESETZ is blinking, you are…
Hello Chayma,
You have to build an adapter board from HDMI to RGB888. You may use receiver chip such as the ITE6801.
For example implementations of the ITE6801, you can refer to other EVM reference designs (take the DLP2010 EVM for example). This…
Lucy,
To interface HDMI with the DLPDLCR2000EVM you will need to implement an HDMI receiver, such at the ITE6801. Example implementations of this can be found in the reference design for our DLPDLCR2010EVM, which has an onboard ITE6801 HDMI receiver…
Hello Alex,
If you are able to find a way to run it, all the .exe contains is a clickwrap license required to be agreed to before using the code.
We do not have a DLPC3435 I2C command to turn on PROJ_ON since it is an input to the device. However…
Dear Fizix,
Thanks a lot for your reply.
I wonder if I could use the TIDA-00384 ( http://www.ti.com/tool/TIDA-00384?keyMatch=null&tisearch=tidesigns ) or TIDA-00325 ( http://www.ti.com/tool/TIDA-00325?keyMatch=null&tisearch=tidesigns ) as the SLM…
Roshan,
Welcome to the E2E forums, and thanks for your interest in our DLP technology.
It's very likely that you've damaged something on the device. There are several voltage regulators which may or may not be working anymore, as well as a power management…
Divyesh,
Unfortunately the datasheet for the HDMI receiver is not available online. You have to request the datasheet directly from ITE.
As for pinout/implementation of the chip, I recommend you review our EVM reference designs on TI.com. This will…
Hello!
Thanks for using the DLP E2E forums. Information should be in the design files section of the below TI design.
www.ti.com/.../tida-00325
Best,
~Danny W
Hello User,
Welcome to the E2E forum and thank you for your interest in DLP® technology.
Please allow me to address your questions.
Jerome Beguin said: - Can I use the CYUSBS236 from cypress ?
Yes, but please note that this is a development tool…