Jeff,
Let me try to answer your questions individually.
> Information regarding the DLP2010EVM reference design, which includes schematics, BOM files, and gerbers, can be found here: http://www.ti.com/tool/tida-00325
> For layout considerations…
Part Number: DLPDLCR2010EVM
Dear DLP Customers and E2E Users,
As of the writing of this post, DLP Lightcrafter Display 2010 EVM (DLPDLCR2010EVM) has reached end of life (EOL) state and is no longer available for purchase from TI.com. Here, we will…
Hello Cris,
The chipset is designed to operate when properly configured with the DMD, controller, and PMIC/LED driver. In your case you should connect the light engine (which I believe uses a DLP2010 DMD) for proper startup with the DLPC3435 and DLPA3000…
Hi Andy,
Thank you for sharing your requirements. This is very helpful. TI is currently developing DLPC3470 controller targeted for light control application. The DLPC3470 controller and DLP2010 DMD will meet your system requirement.
You can preview…
Lars,
No, you do not need to design the board from scratch yourself. Rather, you should adapt the existing board design we provide for users on TI.com.
The DLPDLCR2010EVM, which is linked below, allows for evaluation of the chipset. It implements…
Henrik,
If you want to go from HDMI to RGB888 (as used by the DLP2000 EVM) the easiest way would be a receiver chip such as the ITE6801 (which is what we often use in these sorts of applications). Unfortunately the manufacturer provides limited information…
Hello Manuel,
You can create your own adaptor board for the flex cable. With the footprint of the flex connectors, you can design our own extension. This link will give you the information you need.
http://www.ti.com/tool/tida-00325
Also, make sure…
Leonardo,
I trust that you are doing well.
The web page for the DLP 2010 EVM features a link to the reference design, which includes schematics and a BOM. I have provided a link here for your convenience: www.ti.com/.../tida-00325
Please scroll…
Hello Samtim,
You can backup the .img file from your DLPDLCR4710EVM. Please use the GUI and click on backup firmware. Please let me know if you have any questions.
The DLPDLCR2010EVM has audio included on the EVM. You can take a look at the schematic…