Other Parts Discussed in Thread: TIDA-00335 , UCC25600 The introductory section of the reference design document for the TIDA-00335 power supply mentions an optional microcontroller, "The design also provides flexibility for battery voltage and current…
The schematic for this on the web site is a very simplified block diagram, not the actual board design schematic pdf. is it possible to get the real schematic to see more of details and supporting parts used?
Thanks,
Steve Sturges
Hi Harry,
Actually, TIDA-00335 is reference design and is not orderable.
But you can use the Gerber or CAD files for manufacture with BOM available on TIDA-00355 Page.
Thanks.
Hello Richard,
The calculations in the pdf look correct. As a reminder, these calculations were done only with the resistive network in mind. No other components were taken into consideration, especially when measuring the Insertion losses. As mentioned…
Hi,
There are no specific guidelines for developing a non-Qi system. Our products will work well in that condition. The communication protocol and power transfer will remain the same. For example, the TIDA-00335 transmitter follows all of the protocols…
Hello Nir,
After looking at the schematics, I believe that the decrease in the LO and image rejection may originate from the I/Q inputs which are given. Sideband supression depends on how well the phase and amplitude of the I/Q signals are in match…
Saad:
There is a TI Design in the works that uses the DAC38RF82 as an I/Q source to support very wide bandwidth signals. The TI Design number is TIDA-01435. This design is not currently released as of 7-10-17 but will be in a few weeks. In the mean…