Part Number: TIDA-00362 Other Parts Discussed in Thread: DLPLCR4500EVM , TIDA-00384 , TIDA-00325 Hi,
I would like to use the digital micromirror device as the spatial light modulator (SLM) which is illuminated by the external laser source. Could you…
Part Number: TIDA-00362 Hi
My question is about reference design file of dlp6500 :
Is there any way to connect two camera to evm board?
If yes. hows the calibration process and other work to do?
Part Number: DLP3010EVM-LC Other Parts Discussed in Thread: DLP4710EVM-LC , TIDA-00362 , DLPC3478 , TIDA-00361 Tool/software: Hello support team,
I recently purchased the DLP3010-LC EVM for use in a 3D development project. I have referred to several…
Hello Mostafa,
Please review this TI Design with software to see if it meets your design requirements: http://www.ti.com/tool/tida-00362 .
Here are some additional references to explore: http://www.ti.com/lit/ug/dlpu019b/dlpu019b.pdf ,
http://www…
Hi,
Welcome to E2E forum.
To provide our best suggestion, can you please provide your requirement in detail. From windows through python script, which hardware will be triggered.
Sending trigger in pulses from python script to DLPC900 controller…
Hi, Fizix!
Thank you very much for your efforts on this one, especially during the Christmas time!
For sure I never run FlyCapture2 dashboard in parallel with TIDA-00362 scanner build.
I'll recalibrate the system once again making screenshots…
Other Parts Discussed in Thread: TIDA-00362 , TIDA-00254 I'm new in this argument. I see tida-00254 and tida-00362 design, but i don't understand if i can add two cameras and how can i add a motor two rotate the object.
i need to build a 3d scanner…
Amir,
Can you please tell me if the hardware has been modified?
I would recommend that you download the reference design for the Lightcrafter 6500 - this will give you the schematics for the board and let you know where to probe for those signals…