Part Number: TIDA-00362 Other Parts Discussed in Thread: DLPLCR4500EVM , TIDA-00384 , TIDA-00325 Hi,
I would like to use the digital micromirror device as the spatial light modulator (SLM) which is illuminated by the external laser source. Could you please…
Part Number: TIDA-00362 Hi
My question is about reference design file of dlp6500 :
Is there any way to connect two camera to evm board?
If yes. hows the calibration process and other work to do?
Hello Mostafa,
Please review this TI Design with software to see if it meets your design requirements: http://www.ti.com/tool/tida-00362 .
Here are some additional references to explore: http://www.ti.com/lit/ug/dlpu019b/dlpu019b.pdf ,
http://www.ti.com…
Hi, Fizix!
Thank you very much for your efforts on this one, especially during the Christmas time!
For sure I never run FlyCapture2 dashboard in parallel with TIDA-00362 scanner build.
I'll recalibrate the system once again making screenshots while…
Part Number: DLPC900 Other Parts Discussed in Thread: TIDA-00362 , TIDA-00254 Hi,
I am following the instructions for setting up the DLP ALC SDK, and when compiling the Machine Vision 4500 application, I keep getting this error:
It seems to be something…
Part Number: DLP-ALC-LIGHTCRAFTER-SDK Other Parts Discussed in Thread: TIDA-00362 , TIDA-00254 , TIDA-00361 My development environment is x64 and windows 10. I tried to build alc-sdk following dlpu042 manual but replacing mingw32 by visual studio 2015(64…
Hi Jaap,
Welcome to the DLP Forums and thanks for your question! There is a flaw in our user's guide that needs to be corrected - in order to successfully compile the ALC SDK, you also need to have installed the Flycapture SDK from FLIR/Point Grey. The…
Other Parts Discussed in Thread: TIDA-00362 , TIDA-00254 I'm new in this argument. I see tida-00254 and tida-00362 design, but i don't understand if i can add two cameras and how can i add a motor two rotate the object.
i need to build a 3d scanner…