Part Number: TIDA-00366 Other Parts Discussed in Thread: TIDA-00364 , Hello, both mentioned reference designs probably can be used as a basis to prototype our motor controller. Yet they are different mostly in terms of Isolation/non-isolation and also…
Part Number: TIDA-00366 Other Parts Discussed in Thread: TL431 But How TL431 is able to generate 5V as VDD1, since the cathode is connected to 16V(or 15V) wrto U_TOP_REF, while the AMC can take maximum 6mA of current, to have 11Volts drop across resistor…
Part Number: TIDA-00366
Hi all Would you mind if we ask TIDA-00366? We developed the board which is very similar with TIDA-00366 desgin. As the different point, there is the difference IGBT module only. The voltage conditions are follows; VDC+ and VDC…
Part Number: TIDA-00366 Other Parts Discussed in Thread: UCC21520 , TL431 , AMC1301
UCC21520 Vdda is given at 16V using Bootstrap while the net VCC_U will also be at 16V w.r.to U_TOP_REF. but VCC_U is also used for giving supply for ADC using TL431…
Other Parts Discussed in Thread: TIDA-00366 , TIDA-00736 Hi TI Experts,
I am looking for the sample code for TIDA-00366 and TIDA-00736. Would you please provide them to us?
Best regards. Kaka
Part Number: TIDA-00366 Currently developing a motor controller using the TI TIDA-00366 as reference design. We have one question on that specific design:
The design shows a +16V_GPS input (16V gate drive input voltage) that is required in addition…
Part Number: TIDA-00366 Other Parts Discussed in Thread: TIDA-010006 , LM3480 , TIDA-01420 , AMC1311 , AMC1301 , , UCC21530 , ISO224 , ISO122 Hi,
I am trying to design a 15-20kW AFE motor drive, which consists of an active rectifier and an inverter…
Part Number: TIDA-00366
Hello!
According to the schematic of TIDA-00366 , at the starting point it's clear that bootstrap capacitors aren't charged.
So AMC1301 IC's used for three-phase current sensing are not supplied because their VDD1 are supplied…
Part Number: TIDA-00366 Other Parts Discussed in Thread: AMC1301 , OPA320 , TLC372 , UCC21520 Hello!
According to the schematic of TIDA-00366, at the starting point it's clear that bootstrap capacitors aren't charged.
So AMC1301 IC's used for three…
Part Number: TIDA-010025 Other Parts Discussed in Thread: TIDA-00366 , Hi, I was designing a 3 phase inverter(750VA) for a three phase 500W motor load application. I found some TI reference designs TIDA-010025 and TIDA-00366, which are designed for the…