Hello,
I reproduced the tida-00374 board but when I try to program the CC2650 installed there by smartrf06 and flash programmer, the chip is recognized but the flash size results 0k and the programming fails (as well as flash reading). I checked the…
Hello,
I reproduced the tida-00374 board but when I try to program the CC2650 4x4 installed there by smartrf06 and flash programme 2, the chip i think is not recognized, even it results "connected", the package size detected is 5x5 and the flash size…
Other Parts Discussed in Thread: CC2650 Hi all,
I reproduced the tida-00374 board (with just little changes) but when I try to program the CC2650 4x4 package installed there through smartrf06 and flash programme 2, the chip i think is not recognized…
Other Parts Discussed in Thread: CC2650 , TIDA-00374 Hi,
I want to create a wireless temperature & humidity sensor based on the CC2650 to run on AA batteries for up to 5 years. TI have released a good reference design for this with 10yr life however…
Hi Jack,
Sorry for the delay in the answer.
For your purpose you can use the example code of TIDA-00374. It is originally developed for the HDC1000, but it can be used also for the HDC1010. You can download the source code from TIDA-00374 TI design…
Other Parts Discussed in Thread: TIDA-00374 , CC2650 Hi,
I'm reading TIDA-00374 and TIDA--00484 design documents.
It's very interesting to use coin cell battery for BLE or Sub-1 GHz sensors more than 10 years.
But I'm using ZigBee, CC2650.
Is…
Other Parts Discussed in Thread: TIDA-00374 , CC2650 , CC2560 , CC2640 Hi,
I've no experience yet with TI microcontroller.
I've done a board with the CC2650 microcontroller based on the TI reference TIDA-00374
So far, the power seems to be good…
Hi Tzuyu,
You can find the reference source code for using the HDC1000 with the CC2650 MCU in the TIDA-00374 TI design webpage:
www.ti.com/.../TIDA-00374
You have to download and install the source code files from the following link:
www.ti…