Part Number: DRV10983 Tool/software: Code Composer Studio hello
i am bldc ceiling fan manufacturer
currently i design my ceiling fan on drv10983
all parameter is work correctly
i have one problem is i require a turnoff button in remote
currently design…
Hi Marvin,
We have a reference design for ceiling fans which uses MSP430G2201 processor to decode infrared signals for speed control. Here's the link.
https://www.ti.com/tool/TIDA-00386
Regards,
Vishnu
Other Parts Discussed in Thread: TIDA-00386 , PMP9643 Hi,
I would like to know the manufacturer part no. or complete electric & mechanical specification of the transformer part (RM10/I - P-1031 5-pin Bobbin Renco Electronics) used in this reference design…
Other Parts Discussed in Thread: TIDA-00386 , DRV10983 Hi,
My name is sean.
There are questions about TI_DESIGN_TIDA-00386( http://www.ti.com/tool/TIDA-00386?keyMatch=drv10983&tisearch=tidesigns ).
1) ADC POWER output voltage to change from 24V to 25V…
Part Number: DRV10983 Hello,
I have a custom board for DRV10983 paired with MSP430 G2352. I am using an external 4.75K pulldown resistor for DIR pin as per the reference design ( TIDA-00386 ). But i can't change the direction on giving a High command at…
Hello Yunsheng,
Yes I am aware about UCC28630 . In fact, I used it TIDA-00386 BLDC ceiling fan design during my tenure in TI.
My present application is automotive, UCC28600 is AECQ100 qualified but UCC28630 not. UCC28700 is also AEC qualified but bit costly…
Part Number: DRV10983 Other Parts Discussed in Thread: TIDA-00386 , DRV10987 , , PMP9643 Hi,
In reference to the Ref. design TIDA-00386, I have following queries :
1. What is the Power Factor in this design? I am not able to get the Power factor in the…
Hi Jigar,
Thanks for providing the details. I believe the AC fan regulator that you mentioned in the block diagram is a transformer. The TIDA-00386 can be modified by replacing the proposed transformer in TIDA-00386 with your transformer (AC fan regulator…
Hi Jonathan,
Thanks for posting your question in MD forum. Do you know the rated motor voltage? You mentioned the drive voltage is 180-280V AC so if the Motor voltage is between 6.2 and 28V, DRV10987 will be a good option. We have a reference design …
1) You can choose a motor driver that meets your needs through this link. www.ti.com/.../products.html .
Here is an example filter results page: www.ti.com/.../products.html
2) Like you said, DRV10975 provides constant duty cycle/torque control, but…