Part Number: TIDA-00489
Tool/software: Code Composer Studio
Hey guys,
in the Sub 1GHz forum, I was asked to check the Tx frequency accuracy of our TIDA board, since we had issues with the caps of our 32kHz crystal. We used different transmission modes…
Stefan,
There are pre-built configurations in the project to set the correct project settings.
After you import the project, right click and go to "Properties". Click on "Build". On the top, you should see configuration section. On the right of the…
Part Number: TIDA-00489 Other Parts Discussed in Thread: CC1310 Tool/software: Code Composer Studio Hello everybody,
I have a question regarding the possibilities to flash the TIDA-00489. From the PDF document http://www.ti.com/lit/ug/tiduau1b/tiduau1b…
Part Number: TIDA-00489 Other Parts Discussed in Thread: CC1310 Hey guys. We have encapsulated approx. 25 TIDA 00489 modules with resin (I currently do not know the exact name of the resin, if you need it let me know). The TIDA modules were placed into…
Part Number: TIDA-00489 Other Parts Discussed in Thread: CC1310 Hey guys we are using TIDA 00489 layout and I have some questions regarding production.
We want to use a CLI script to flash our software on the CC1310 and we have to readout the MAC address…
Part Number: TIDA-00489 What is the maximum input voltage for the TIDA-00489?
To expand the lifetime at higher current consumptions, I want to change the coin cell holder with a regular AA-Battery holder and supply the device by a 3.6V Lithium Battery…
Part Number: TIDA-00489 Hey guys,
we are planning to manufacture PIR sensors using the TIDA 00489 design. We will need a test bench to ensure the produced sensors are working.
We are currently planing test pins:
VCC
GND
Comparator outputs (low and high…
Part Number: TIDA-00489 Other Parts Discussed in Thread: CC1310 Hey guys,
we are using the TIDA 00489 layout and have some test sensors here (no changes made to layout). We are counting the movements detected by the sensor using HWI and increment a counter…
Part Number: TIDA-00489 Other Parts Discussed in Thread: CC1310
Tool/software: TI-RTOS
I am working with cc1310
I need to monitor the battery in mV
My code is,
int get_bat_status(void) { uint32_t bat_volt;
float bat_status=100.0;
if(AONBatMonNewBatteryMeasureReady…
Part Number: TIDA-00489 Hey guys,
we have some issues with the TIDA 00489 PIR sensor design. We noticed, that during tests the sensor was heavily influenced by a dimmed LED ambient light. We are counting the movements in a room for 5 mins. If the LED…