I don't think you can order the TIDA-00652 reference design. However, the design files are available in the product folder page ( www.ti.com/.../TIDA-00652) to print and assemble the board yourself.
also regarding the solar panel circuit, I'm guessing…
Hi Dinar,
I suggest testing the TIDA-00652 as a stand alone power supply first to ensure there are no issues with its output voltage. It would also help if you could post waveforms of the 24V output from the TIDA-00652 when the system is not working…
Part Number: UCC28180 Other Parts Discussed in Thread: DRV10983 , MSP430F2274 , TIDA-00652 Hi
I have built Buck converter using reference design TIDA-00652, it gives 23.95Volt and I have build a break out board for DRV10983 which works fine when the…
Part Number: DRV10983 Other Parts Discussed in Thread: TIDA-00652 , Hello everyone
I am trying to power a MSP430G2231IPW14 , through DRV10983 , I have used the standard circuit a provided on TIDA-00652, the Voltage at V3P3_Reg, drops to 2.9V, and DRV…
Hi Tomer,
Thank you for your interest in the UCC28019A. That does fit nicely in the power range you highlighted. The UCC28180 is also a popular product at that power level.
1. Yes, it will meet IEC-61000-3-2. Note section 7.1 (p10) and 8.1 (p20) in…
Part Number: DRV10983 Other Parts Discussed in Thread: USB2ANY , TIDA-00652 Hi TI support Team,
I am observing the below error with USB2ANY and DRV10983 (TIDA-00652).
I have updated the USB2ANY firmware but still observing Register writing failure…
Part Number: UCC28180 Other Parts Discussed in Thread: TIDA-00652 , Hi team,
My customer is looking for an in depth explanation of how this particular circuit operates in the attached reference design. Can you explain, or point out where in the reference…
he optocoupler input is full wave rectified AC and not DC. With increase in amplitude the current increases in optocoupler. As the triac fires at different phase, a PWM signal is generated accordingly at the output of optocoupler.
To learn more about…
Part Number: DRV10983 Other Parts Discussed in Thread: MSP430G2231 , TIDA-00652 Dear team,
We are trying to work on the BLDC fan based on ref design: TIDA-00652. Please help to provide the sample codes for MSP430G2231 as how to drive the DRV10983? …
Hello John,
I reviewed the UCC29910 data sheet and the block diagram is hard to figure out. I also could not find any application material on the device and can see the device was released in 2011. I will discuss this with my colleagues to see if…