Part Number: TIDA-00913 Hi, I'm using Intanspin-FOC for an application with more than two motors. Motor 1 and 2 are spinning correctly, but when I try to start a third observer using "obj->estHandle = EST_initEst(MTR_3);", it doesn't work. Is there a…
Part Number: TIDA-00913 Tool/software: Hi Expert,
This is for Compal ORV3 management board, end customer is Dell.
Customer asked for the DC/AC solution for liquid cooling motor.
I've proposed TIDA-00913 but customer need single phase solution. …
Part Number: TIDA-00913 Other Parts Discussed in Thread: BOOSTXL-3PHGANINV , C2000WARE , MOTORWARE Dear team:
This development board is used to detect the output current, and its matching routines are sampled at the following time:
PWM_setSocAPulseSrc…
Part Number: TIDA-00913 Other Parts Discussed in Thread: INA240 , TMS320F28069M Hello,
In the TIDA-00913 reference design, there is a RF filter in the output of INA240 and there is no input filter before the INA240.
1-)When should we use that RF(output…
Part Number: TIDA-00913 Other Parts Discussed in Thread: LMG5200
What GaN evaluation boards/ power module have feeadback option ?
Is possible to control/adjust frequencies to 42.8 KHz, 21.4 KHz and 10.7 KHz ?
pulse with 2.5%,5%, 10% is…
Part Number: TIDA-00913 Other Parts Discussed in Thread: INA240 , TMS320F28069M Hello,
The following picture is in the TIDA-00913 reference design:
I have some questions about that:
1-)What we can do for avoidance of reading those transient events…
Part Number: TIDA-00913 Other Parts Discussed in Thread: INA240 Hello,
What is the benefit of having three INA240 inline sensors instead of having two ?
Regards,
Mohammad.
Part Number: TIDA-00913 Other Parts Discussed in Thread: LMG5200 , TIDA-00915 , DRV8412 , DRV8844 , DRV8704 Our customer is looking for 48V single phase inverter solution.
Power range is up to 50W.
Do you have any solution or reference design for…
Part Number: LMG5200 Other Parts Discussed in Thread: TIDA-00909 , TIDA-00913 , INA240 ,
Hi!
Does anybody know if there is any difference between reference designs TIDA-00909 and TIDA-00913. It looks like it is a same desing, but the report focuses…
Part Number: TIDA-00913 Other Parts Discussed in Thread: LMG5200
In order to avoid the interference of power part to signal part, NT1 is used as the connection point form AGND to PGND.In order to make the driving signal electrically stable relative…