Part Number: TIDA-00951 Hello, I've submitted the request for software download for TIDA-00951 three times in the last 20 days. and i cant get it yet.
as well as i have looked at my junk mail and my mail box carefully.
Part Number: TIDA-00951 My customer is asking to get an evaluation board to do the test. Is that possibly team could support this board?
Application: Motor Drive
Use case: Bi-direction DC/DC charger for DC Link and 24V system backup.
Very thanks.
Brian…
Part Number: TIDA-00951 Other Parts Discussed in Thread: TIDA-01159 , TIDA-01281 Hi,
I am using Tıda-00951 2-kW, 48- to 400-V,Isolated Bidirectional DC-DC Converter with Tıda -00951 software, programming of the control card with the appropriate software…
Part Number: TIDA-00951
Hi,
is there any analysis available about part efficiency in the design and how to improve it (FET, transformer, snubber).
As I can see the transformer is very hot already at 1.5kW. The efficiency is >93%. Würth changed the…
Part Number: TIDA-00951 Hello,
I am writing to ask about the design and control of tida-00951. At the end of the reference design, Section 11, several research papers and documents are listed as related to the reference design. Could you please advise…
Part Number: TIDA-00951 Other Parts Discussed in Thread: TMS320F28335 , , TIDA-01281 Hello,
I am writing to ask about controlling tida-00951 using TMS320F28335. I saw another posting (with its link below) that the code is packaged in libraries. Does this…
Part Number: TIDA-00951 Hello,
I have a question regarding the operation of tida-00951. In the reference design document, in table 1 (key system specification), it is mentioned that in battery charger mode, the input current (I_bus_max) is 60A. If this…
Part Number: TIDA-00951 Hi
When I follow step by step of this design, the equation # 9 seems like not right. The ITXpri_rms can not be 47A.
Please let me know.