Part Number: TIDA-010006 Other Parts Discussed in Thread: LM5180 Hi,
We have a customer whose requirements are similar to TIDA-010006, below are their requirements.
Input: DC20V +/-10%
Output 1: DC20V/120mA.
Output 2/3/:DC15V/50mA each of them.
…
Hi Victor,
I am following up this old thread. We don't have any spare TIDA-010006 reference design.
To enable customers build a prototype of a TI reference design such as the TIDA-01006, we provide the entire Altium CAD files https://www.ti.com/lit…
Hi Nicholas,
A single flyback converter with multiple output windings similar to TIDA-00199 or TIDA-010006 can be used for generating the gate drive voltages.
For higher power output motor drive inverters like TIDA-00917 it is better to use multiple isolated…
Part Number: LM5180 Other Parts Discussed in Thread: TIDA-010006 Tool/software: WEBENCH® Design Tools Hello, I used LM5180 TINA model which is found in the link below.
https://e2e.ti.com/support/tools/sim-hw-system-design/f/234/p/814419/3026928?tisearch…
Part Number: LM25019 Other Parts Discussed in Thread: LM5019 , TIDA-010006 This spec falls under the isolated flybuck converters line but I don't see any information regarding the isolation specs on the datasheet. Is it rated for 1.5kVrms or 3kVrms isolation…
Part Number: TIDA-00366 Other Parts Discussed in Thread: TIDA-010006 , , TIDA-00199 Hi,
I see you used two power supplies in this design. One 16V and another 5V. Why didn't you make 5V from 16V rail? what was the point for having two supplies?
Thank…
Hello Mohsen, You can refer to TIDA-010006 for generating isolated supply rails for the gate drivers. For 15v to 5v conversion, please refer to TIDA-01420 on using LM3480.
For grid voltage sense you can consider using AMC1311.
regards
Navaneeth
Hi,
Seems like i was able to generate a design using webench
webench.ti.com/.../SDP.cgi
Alternatively you can take a look at this TI design for multiple rail using LM5180
www.ti.com/.../TIDA-010006
Thanks
-Arief