Part Number: TIDA-010038 Hi Team,
My customer is developing an Inverter solution. I suggest them to reference our TIDA-010038. They would like to get source code for reference. May I know where can I get the source code? Thank you.
Best regards,
Mik…
Part Number: TIDA-010038 Dear Support,
Continuing the previous thread, we decided to follow your suggestion and ordered a new transformer made for us for this application. We measured the secondary turns ratio to be approx. 6.8.
Unfortunately, we have some…
Part Number: TIDA-010038 Dear Support,
We are trying to implement the TIDA-010038 reference design with some modifications; the main one is having a temperature dependent output voltage. The voltage range required is 26.5V to 29.5V (temperature optimized…
Part Number: TIDA-010038 Hi!
i am reading the reference design TIDA-010038 for charger which has PFC and LLC stages of charging. but it as some limitation and because of these limitations i cannot use it in my design.
I want to design same type of charger…
hi,
In ST application note AN2644, they recommended a split capacitor configuration to solve startup issues. Comparing the EVM with TIDA-010038, the EVM has an additional capacitor installed on their board and schematics. See below. After adding the capacitor…
Part Number: TIDA-010038 Hi,
I am building an SMPS with similar specs as the TIDA-010038 reference design. This reference design draws about 0.4W without load. However this SMPS is supplying power to my circuit that draws about 10mA during standby. The…
Part Number: TIDA-010038 Hi Experts,
My costomer wants a power reglator by LLC topology.
I am useing the UCC256404 LLC controller.
Target is trying to get output from 0V to 150VDC enable to achieve the CC/CV design.
I want to ask about the TIDA-010038…
Part Number: TIDA-010038 Hi,
My customer is designing a SMPS following this design. He is unable to find the spec of this L2 (200uH 750316570 Wurth Elektronik).
Can you help to provide ?
Another question. What is the purpose of this current sense circuit…
Dear Sir/Madam,
My customer is interested to evaluate TIDA-010038, but this eval kit is not open for sale.
Is there anywhere we can get the evaluation kit to customer to kick start the evaluation instead of building from schematic and BOM provided.
…
Part Number: TIDA-010038 Hi TI team,
Customer reviewed TIDA-010038. they try to design a charging system.
Battery : 48V
Charging voltage : 55V
Charging current : min 0.2A, typical : 0.4A, max : 0.5A
1. Do you have a sheet for calculating the parameter…