Part Number: TIDA-010054 Hello TI Expert,
I am using the TIDA-010054 DAB reference design and am looking for the PLECS simulation models used for this design.
Could you please advise if these files are available for download?
Thanks,
Krishna…
Part Number: TIDA-010054 Tool/software: Where can I buy TIDA-010054 evaluation board ?
Have need additional board to work with TIDA-010054 ?
Thanks you
Part Number: TIDA-010054 Please explain the concept of capacitance value. There are 14 pieces of 0.47uF capacitors installed on one side, totaling 6.58uF. If this total capacitance were very small, for example 0.1uF-0.6uF, what kind of impact would it…
Part Number: TIDA-010054 Tool/software: use tidmax5b.zip TIDA_010054_DAB_standalone.plecs
I change the EPS_EN =0
Or EPS_EN =1
See the output Ipri,Isec ,output I ,and ,output V
Looks no any difference
Why EPS_EN no useful?
May I needs change…
Part Number: TIDA-010054 Tool/software: Hello TI Team,
I’m reviewing the reference design TIDA-DAB-010054 and noticed that the gate drive loss is calculated using the formula:
Pgate=2⋅Qg⋅(VDD−VEE)⋅fsw P g a t e = 2 ⋅ Q g ⋅ ( V DD − V EE )…
Part Number: TIDA-010054 Hello, I am using TIDA-010054 to design a bidirectional Dual Active Bridge dc-dc converter. I have your reference guide and successfully completed the Lab 01. However, when I moved forward to Lab 02, I am getting DAB_tripFlag…
Part Number: TIDA-010054 Hello everyone
I am currently working on Dual active bridge converter for 50kW application . based on the reference design TIDA-010054 . was able to achieve ZVS but the issue i was facing with ltpsice simulation if i am decreasing…